Interconnect Design for Defense UAVs and SWaP Optimization
How Interconnects Affect Defense UAV Performance and Reliability

(Source: Grispb/stock.adobe.com)
Published August 5, 2026
Uncrewed aerial vehicles (UAVs) are taking on a growing range of defense missions, from intelligence, surveillance, and reconnaissance (ISR) to communications support and logistics. Each new capability typically adds another sensor, processor, radio, or payload. The challenge is integrating more technology into the aircraft without sacrificing flight time, maneuverability, or payload capacity.
Investment in uncrewed systems continues to grow across the defense sector. Analysts estimate that the global counter-drone market is worth between US$3 billion and US$7 billion today and could reach US$14.5 billion by 2030.[1] Although this forecast focuses on counter-drone technologies, it reflects the broader growth of the systems and infrastructure that support uncrewed operations.
When new capabilities are added to UAVs, they often require additional interconnects and interfaces. As system complexity increases, the connectors, cables, and interfaces that link them together can affect size, weight, and power consumption (SWaP), as well as reliability and long-term mission capability.
This blog explores how interconnect technologies help reduce SWaP requirements while supporting the data, power, and reliability needs of modern defense UAVs.
The SWaP Impact of Interconnect Design
When it comes to UAV design, every ounce matters. Engineers have spent years trimming weight and conserving space by improving airframes, batteries, propulsion systems, and other electronics. Interconnects offer another opportunity to make the most of the limited space inside a UAV.
SWaP is closely tied to overall aircraft performance. Every reduction in weight gives designers more flexibility, whether the goal is longer flight times, greater payload capacity, or more onboard computing resources. Minimizing connector size and weight frees valuable board space for additional electronics, such as sensors, communication modules, or mission-specific electronics for UAVs.
Modern UAVs may include cameras, radar systems, Global Positioning System (GPS) receivers, communications equipment, onboard processors, and mission-specific payloads. Each requires power and data connections, yet they compete for the same limited space and weight budget.
Smaller connectors and cable assemblies can reduce weight and free up valuable space inside the aircraft. Compact RF interconnects can also shorten cable runs, helping to preserve signal quality and simplify cable routing.
Reducing SWaP can enable longer deployments, improve fuel or energy efficiency, and increase capacity for surveillance and other mission equipment.[2] Even small reductions in connector size and weight can add up in a space-constrained UAV design.
Connecting the Modern UAV
Every UAV relies on a network of interconnects to transmit power, data, and communication signals. A camera capturing imagery, a processor analyzing data, a radio transmitting information, and a motor driving the aircraft all depend on reliable electrical connections.
All UAVs depend on a reliable source of power. Energy from batteries or onboard generators must reach flight controls, propulsion systems, communications equipment, and mission payloads while minimizing voltage drop and unnecessary losses.
Once power reaches these systems, they must reliably exchange information. High-speed digital interconnects transfer large volumes of sensor data between cameras, processors, storage devices, and AI accelerators. Higher-resolution sensors and onboard AI systems generate large amounts of data, requiring interconnects that support high data rates while minimizing noise and signal degradation.
Some of that information remains within the aircraft, but communication systems must also transmit data beyond the airframe. RF interconnects are critical for communications, satellite navigation, telemetry, radar, and electronic sensing systems. For reliable wireless performance, it’s important to maintain low insertion loss while controlling electromagnetic interference (EMI). This is especially important when multiple radios operate simultaneously within a confined UAV airframe.
In applications where bandwidth requirements are growing, some platforms incorporate fiber-optic links to support high-speed data transmission. Fiber-optic connections can carry large amounts of data and are immune to EMI from motors, power electronics, and onboard radios. This combination of high bandwidth and EMI resistance makes fiber optics a valuable option for demanding UAV applications.
Sensor payloads introduce additional connectivity requirements. Cameras, light detection and ranging (lidar), radar, hyperspectral imaging systems, and other mission equipment require power and data connections to the aircraft. Many platforms are expected to support changing payloads throughout their service lives, making standardized electrical and mechanical interfaces essential for integration and future upgrades.
Those same connections support maintenance and mission preparation activities. External I/O interfaces provide access for diagnostics, software updates, charging, and servicing. Because these connections are used frequently, they must withstand repeated mating cycles and endure harsh environmental conditions.
Requirements such as signal integrity, impedance control, current-carrying capability, EMI performance, bandwidth, and routing density influence connector selection across all these paths.[3] Improving one area may affect another, making interconnect design an important part of the overall system architecture.[4]
Ruggedization, Modularity, and Maintainability
Unlike many commercial drones, defense UAVs often operate in environments where connectors are exposed to vibration, thermal cycling, shock, moisture, dust, and EMI. To maintain reliable connections under these conditions, interconnect systems must be designed for harsh operating environments.
This becomes more difficult as aircraft become smaller and lighter. Reduced structural mass can transmit more vibration to onboard electronics, increasing demands on connector retention and contact durability. Connectors must maintain reliable performance under these harsh conditions.
In addition to surviving harsh conditions, many UAVs are expected to support evolving missions throughout their service lives. Modularity has become increasingly important as UAV missions evolve. Open, standardized interfaces simplify payload replacement and enable operators to configure aircraft for surveillance, communications, mapping, and other specialized missions without extensive redesign. Standardized interfaces can also reduce integration effort and make future upgrades easier to implement.
Modularity offers benefits beyond mission flexibility. According to the US Government Accountability Office (GAO), operating and support (O&S) costs account for approximately 70 percent of total mission-system life-cycle costs.[5] By simplifying inspection, replacement, and repair, modular systems can help reduce long-term costs while improving platform availability.[6]
The TE Connectivity Wildcat Connector family is an example of an interconnect solution designed for these environments. Engineered for high-density aerospace and defense applications, Wildcat connectors combine a compact footprint with ruggedness to withstand vibration and other demanding operating conditions. Their modular design supports integration into space-constrained UAV platforms.
Connectivity as a Capability Enabler
Every connector, cable, and interface occupies space and adds weight to a UAV. Selecting the right interconnects helps engineers manage SWaP constraints while supporting the power, data, and communications requirements of increasingly more capable aircraft.
Interconnect design also affects how easily payloads can be integrated, upgraded, and maintained over time. In modern UAVs, connectivity is more than just making connections. It is part of the overall balance between capability, reliability, and SWaP.
[1]https://www.reuters.com/business/aerospace-defense/drone-strikes-beyond-battlefield-pump-up-market-technology-repel-them-2026-06-18/
[2]https://www.te.com/en/industries/defense-military/applications/unmanned-aerial-vehicles.html
[3]https://www.te.com/en/industries/aerospace/applications/emi-shielding-drones.html
[4]https://www.te.com/en/industries/defense-military/insights/interconnect-solutions-optimized-for-rugged-environments.html
[5]https://www.gao.gov/assets/gao-25-106931.pdf
[6]https://www.gao.gov/products/gao-26-108140
Author
Bryan DeLuca is a seasoned electronics content creator with a deep passion for demystifying complex engineering concepts. Through years of hands-on experience, he has built a reputation for translating advanced electronics topics into practical, engaging content for engineers, hobbyists, and makers.
Bryan produces technical articles and videos that focus on components, power electronics, additive manufacturing, and the integration of microcontrollers, LEDs, and sensors.