Skip to main content

Quantum Computing What it Can, Cannot and Might Eventually Do

Quantum computing has been discussed for years, mostly as something that exists “just over the horizon.” It’s been important in theory, but still far from a day-to-day engineering reality. But now, what was once largely experimental is becoming a sustained engineering effort. Governments are funding national quantum initiatives.1  Enterprises are experimenting with hybrid quantum workflows, and hardware manufacturers are steadily increasing qubit counts.

At the same time, the expectations around what quantum computing can and cannot do are becoming clearer. Quantum systems behave differently from classical computers. They draw on properties like superposition and entanglement instead of simple binary logic. Unlike traditional computers, which encode data as a system of binary bits (i.e., 0 or 1), quantum computers use qubits that can occupy multiple probabilistic states simultaneously. It is a common misconception that quantum computers are generally faster or better in some way; the reality is that qubits allow computers to approach many different types of computational problems in very different ways than traditional computing.

Understanding the difference is important because quantum computing is not supposed to replace conventional computing or solve everyday workloads. It’s valuable for its targeted applications, long-term infrastructure planning, and more immediate considerations, such as security preparedness. As quantum technology moves out of the lab and into practical applications, engineers need a clear view of its potential and limitations. 

Core Concepts Without the Math


Understanding quantum computing starts with a few basic ideas. Grasping these concepts does not require advanced physics knowledge, but it does require a shift in perspective. Quantum systems behave differently from the digital logic that underlies classical computer processors. Understanding that difference is the basis for understanding both quantum computers’ potential and limitations. Rather than replacing classical computing principles, quantum mechanics introduces new behaviors that can be engineered for specific computational advantages. These differences can be best understood through three closely related ideas: 
•    How qubits differ from classical bits
•    How superposition expands the number of states a system can represent
•    How entanglement allows qubits to work together instead of being isolated units

Qubits vs. Bits

Classical computing bits represent a state of either 0 or 1. A qubit can exist in a superposition of both states at the same time. In Methods: Engineering the Quantum Future, this concept is illustrated as a coin spinning in mid-air rather than resting on heads or tails. 

When multiple qubits are combined, the total computational state space grows exponentially. This exponential growth supports quantum computing’s theoretical advantage for problems in which many possible states must be assessed or constrained simultaneously.

Superposition

Superposition allows quantum systems to represent multiple possibilities simultaneously. This does not mean quantum computers simply try all answers instantly, though. Instead, quantum algorithms manipulate probability amplitudes to increase the likelihood of all possible correct outcomes. This is useful only when algorithms are designed to steer the system toward meaningful outcomes.

Entanglement

Entanglement creates correlations between qubits, so much so that the state of one cannot be fully described without referencing the other. This attribute enables a coordinated computational behavior that has no classical computing equivalent. Together, superposition and entanglement create new computational pathways.

The Current State of Quantum Computing


Quantum computing hardware has made measurable progress in recent years, especially in how qubits are built and scaled. Instead of chasing raw qubit counts, efforts have been more focused on improving reliability and stability. For example, IBM’s current lineup includes processors such as the 127-qubit Eagle and the 133- to 156-qubit Heron family, both built on superconducting qubit technology. The processors incorporate advancements in qubit control, fabrication yield, and modular architecture to improve performance and reliability compared to earlier generations. Heron, in particular, represents IBM’s focus on usable performance rather than just raw scale.2  The highest-performing processor line to date incorporates tunable couplers that reduce cross-talk and improve gate fidelity. These are two metrics that directly determine how deep and reliable quantum circuits can be in practice.

Beyond individual processors, IBM has developed the modular IBM Quantum System Two. The platform is designed to support multiple quantum processing units (QPUs) within a scalable cryogenic environment, enabling hybrid quantum-classical workflows and more real-world experimentation.

The progress in this field is not limited to a single company. Google’s Quantum AI has demonstrated advances in quantum error correction using superconducting qubits. Some of their results show that increasing the number of physical qubits within a logical qubit can reduce error rates.3  This is an important step toward scalable fault tolerance, since systems must continue operating reliably even when individual qubits experience errors. Demonstrating that error rates can decrease as systems scale is necessary to build quantum computers capable of running longer, more complex computations. 

Earlier demonstrations of quantum computational advantage have helped shed light on the areas in which quantum processors can outperform classical systems, specifically in a small set of problems whose mathematical structure aligns well with how quantum hardware operates. 4 

Even so, today’s quantum machines remain noisy intermediate-scale quantum (NISQ) devices rather than fully fault-tolerant computers. The term NISQ, introduced by John Preskill, describes processors with tens to hundreds of qubits that lack comprehensive error correction and remain sensitive to noise and decoherence.5  Quantum states are easily disturbed by their environment, and even small sources of interference can degrade coherence and introduce errors as computations grow more complex.

While recent work has shown that improved error-correction techniques can reduce logical error rates—an encouraging sign for long-term scaling—achieving true fault tolerance requires larger numbers of qubits operating with incredibly low error probabilities.6 This remains an engineering challenge. 

Modern quantum platforms are typically accessed through the cloud and integrated into hybrid quantum-classical workflows. They are not standalone replacements for classical processors but are best understood as specialized accelerators that depend on classical infrastructure for control and most computation.

Key Application Areas Quantum Computing Targets


Quantum computing shows the greatest potential for a small set of problems that classical systems cannot handle. It is not for everyday workloads, such as database queries or routine number crunching. Quantum computing’s advantage lies in problems where the number of possible outcomes grows exponentially—a domain where traditional computational methods lag behind.
These problems often have some common characteristics: They involve enormous numbers of possible configurations, rely on probabilistic behavior, or are rooted in physical processes that are already quantum in nature. In these cases, quantum algorithms offer different pathways to navigate or organize solution spaces that quickly overwhelm classical methods.

Optimization Problems

Optimization is one of the most actively explored areas of quantum applications, largely because it quickly exposes the limits of classical approaches. Many real-world optimization problems involve choosing the best option from an enormous set of possibilities. As more variables are added, the number of potential configurations grows so fast that even well-optimized classical methods can’t keep up.

This challenge appears across a wide range of industries, from routing and scheduling to financial modeling and manufacturing planning. In these settings, the difficulty isn’t just finding a solution but finding a good one within a practical amount of time and within resource constraints. Quantum approaches are being explored for these applications because they offer different ways to navigate these extensive solutions instead of evaluating every possibility one by one. 

Optimization, at this time, is viewed more as an early-use domain for quantum computing because it may help guide classical workflows toward better solutions more efficiently in certain cases, not because quantum systems solve these problems outright. 7

Simulation of Physical and Chemical Systems

Another area where quantum computing gains attention is simulation. Many of the systems that scientists and engineers want to model, such as molecules and chemical reactions, are governed by quantum mechanics at their most fundamental level. Classical computers approximate the behavior, but those approximations become increasingly resource-intensive as systems get more complex.
Quantum computers look at the problem differently. Because they operate using quantum states, they naturally align with the behavior they are attempting to model. This makes them better equipped to simulate molecular interactions and material properties without relying on the layers of approximation required by classical methods.

Quantum computers’ ability to do this has long-term implications in fields like drug discovery, materials development, and semiconductor design because understanding behavior at the atomic level can influence performance, cost, and reliability. Similar modeling challenges appear in areas such as battery chemistry and energy storage, where small changes at the molecular scale can directly influence how a system performs as a whole.

For these reasons, quantum simulation tends to be viewed as one of the most promising long-term applications of quantum computing.8  The practical impact will depend on continued advances in hardware and error correction, but the ability to model complex physical systems more directly is a key motivation behind the ongoing research.9 

Artificial Intelligence and Machine Learning

Quantum computing is also being explored in artificial intelligence (AI) and machine learning (ML), but its role can sometimes be misunderstood. Quantum systems are not positioned to replace today’s deep learning models that rely on mature classical hardware and established training methods. Instead, research has focused on whether quantum computing can assist with specific mathematical operations that appear in some ML workflows.

This type of work, known as quantum-enhanced machine learning (QML), will focus on accelerating certain mathematical operations, like high-dimensional linear algebra and feature mapping, rather than training entire models end to end.

Groups like Google Quantum AI and other academic research organizations continue to investigate these techniques, but practical deployment is mainly experimental. 

Quantum computing for ML is best understood as a specialized tool, not a general acceleration platform. It does not aim to replace AI. Its value lies in complementing classical systems, where certain computations strain classical scaling.

Post-Quantum Security: A Critical Near-Term Concern

Among all potential quantum effects, cybersecurity is the most urgent.
Unlike many proposed applications, the security impact depends less on quantum computers being useful and more on their future ability to break cryptographic systems that are already in use.
Quantum algorithms, such as Shor’s algorithm, indicate that a quantum computer could factor large numbers much more efficiently than classical systems, which many public-key encryption systems rely on. The specifics of this threat and its other potential implications are discussed further in Methods: Engineering the Quantum Future.

In response to this threat, post-quantum cryptography (PQC) focuses on algorithms that can withstand classical and quantum attacks. Transitioning to PQC will require coordination across hardware, firmware, protocols, and network infrastructure.

Even though large-scale, fault-tolerant quantum computers do not yet exist, the urgency stems from the risk that nefarious actors will collect encrypted data now, with the expectation that it can be decrypted later, as quantum capabilities advance. For engineers and system designers, planning for quantum-resistant standards is a present concern.

Engineering Challenges and Realistic Timelines


Even with all the progress underway, quantum computing remains an engineering challenge as much as a scientific one. Developing systems with more qubits is only part of the situation. The qubits must be controlled reliably, protected from noise, and kept coherent long enough to execute useful computations. And this must all be done while operating in cryogenic environments, which present their own set of hurdles. 

Fault tolerance is key among these hurdles. To run long-duration quantum algorithms, systems need thousands of stable qubits that can form more reliable logical qubits. While today’s systems are advancing, they still operate in the noisy intermediate-scale quantum stage. Continued progress is steady, but a fully fault-tolerant quantum computing system remains a long-term engineering goal.

Preparing for a Quantum Future


With the barriers described in this article, quantum computing is not an immediate disruptive technology. It is a strategic infrastructure development, and its impact will build over time as the technology improves. Today, its value lies in experimentation, including using quantum processors alongside classical systems, preparing for quantum-resistant security, and studying applications such as optimization and simulation.

What quantum computing ultimately delivers will depend on how well it scales and how reliable it becomes. Rather than replacing classical computing, it may help address problems that those systems cannot solve. Preparing for this future is a responsible design decision today.

1https://www.quantum.gov/ 
 2 https://www.ibm.com/quantum/hardware 
  3https://www.nature.com/articles/s41586-024-08449-y 
  4https://ai.googleblog.com/2019/10/quantum-supremacy-using-programmable.html 
  5https://quantum-journal.org/papers/q-2018-08-06-79/ 
  6https://www.nature.com/articles/s41586-023-06096-3 
  7https://www.mckinsey.com/capabilities/mckinsey-digital/our-insights/quantum-computing-use-cases-are-getting-real-what-you-need-to-know 
  8https://www.nature.com/articles/s41467-023-43479-6 
  9https://www.nlr.gov/news/detail/program/2025/can-quantum-computers-handle-energy-hardest-problems