Skip to main content

Simplifying High-Voltage DC Power Systems for 400V and 800V Designs

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

Published June 16, 2026

Engineers who develop electric vehicle (EV) battery test systems or semiconductor fabrication equipment need to convert grid power into DC voltages of 400V or higher. Delivering 400VDC or 800VDC typically requires complicated wiring and multiple units to achieve the necessary output. This week’s New Tech Tuesdays explores how integrated high-voltage platforms simplify system design, improve safety, and enhance insights on performance metrics.

Eliminating Architectural Complexity in High-Voltage Systems

Established designs rely on series-stacked power supplies to reach the high voltages required for modern EV battery testing. This approach increases the power rack's physical footprint and creates multiple possible failure points within it. Modern single-chassis platforms provide native 400VDC or 800VDC outputs from a three-phase 180–528VAC input, reducing component counts and streamlining integration. This simplified architecture improves overall system reliability while reducing assembly and maintenance time.

Advancing Digital Control and Diagnostic Visibility

Digital management replaces traditional analog interfaces in high-density power environments, which enables granular control. Standardized protocols, such as Power Management Bus (PMBus), CANopen—a CAN-based higher-layer protocol—Modbus, and Standard Commands for Programmable Instruments (SCPI), allow engineers to monitor real-time diagnostics via a centralized graphical user interface (GUI). These digital features support automated scaling and active current sharing when configuring systems for parallel operation. Precise regulation of constant-voltage and constant-current modes ensures stability under the dynamic load conditions common in plasma generation. High-speed digital feedback loops help the system respond rapidly to load transients. Digital control also enables engineers to perform automated test sequences with high repeatability and lower data latency.

Integrating High-Voltage Safety and Isolation Standards

High-voltage environments demand robust electrical isolation to protect operators and sensitive measurement electronics from hazardous fault conditions. Designing for 800VDC requires careful attention to creepage and clearance distances to prevent arcing. Integrated safety interlocks can disable the output when an access panel is opened or a safety circuit is broken.

Isolated communication channels further protect the control circuitry by maintaining a physical barrier between the logic and power stages. This isolation prevents common-mode noise from disrupting the digital control signals in electrically noisy environments. Meanwhile, hardware-level protections for overvoltage and overcurrent conditions provide a final layer of defense for the connected equipment.

The Newest Products for Your Newest Designs®

The HPT5K0 series, a 5kW programmable AC-DC power supply from XP Power, delivers high-voltage DC outputs and is designed for semiconductor manufacturing, high-voltage testing, and medical applications. The HPT5K0 series offers voltage outputs ranging from 48VDC to 800VDC to meet a variety of high-voltage applications. These units support active current sharing in parallel configurations for scalable power delivery.

Engineers can leverage standard digital protocols, including PMBus, CANopen, Modbus, and SCPI, to integrate these supplies into automated test environments. The HPT5K0 addresses the architectural complexities discussed previously by providing high power density in a single package. Furthermore, its design includes built-in safety features that simplify compliance with industrial standards for high-voltage systems.

Tuesday’s Takeaway

Advancements in high-voltage DC power delivery enable more capable and safer industrial systems. Integrated power platforms remove the need for series stacking while providing superior digital control and isolation. By transitioning to native high-voltage power supplies, engineers reduce system complexity and enhance diagnostic visibility in battery and semiconductor applications.

About the Author

Mouser, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.

Profile Photo of Mouser Technical Content Staff