Skip to main content

A Guide to the EU Machinery Regulation 2023/1230 in 2027

Image Source: Mouser Electronics

By Simon Duggleby, Senior Supplier Marketing Campaign Manager, Mouser Electronics

Published July 2, 2026

The landscape of European manufacturing is undergoing one of the most significant regulatory shifts in two decades. The industry is rapidly approaching the January 20, 2027, deadline for the full application of the EU Machinery Regulation (2023/1230), meaning regulatory changes will be in full motion.[1] Replacing the Machinery Directive (2006/42/EC), the new policy isn’t simply a “software update” that enhances safety rules; it is a total overhaul designed for the age of artificial intelligence (AI), the Internet of Things (IoT), and cybersecurity.[2]

For design engineers and manufacturers, this regulation presents a dual challenge: navigating complex, new legal requirements while maintaining a competitive edge in a market plagued by rising energy costs and labour shortages. However, this transition opens an opportunity. By leveraging the latest semiconductor and sensing technologies from leading manufacturers such as NXP Semiconductors, Amphenol, and Murata, engineers can turn compliance requirements into a catalyst for unprecedented levels of productivity.

What Is the EU Machinery Regulation 2023/1230?

The Machinery Regulation 2023/1230 is the upcoming regulation to be enforced across the European Union, setting mandatory health, safety, and conformity rules for machinery and related products. This new set of regulations seeks to protect workers and consumers from unsafe machinery while allowing the free-flowing movement of products across the EU market. This means that manufacturers, importers, and distributors in the EU are legally obliged to meet the increased safety standards set out in EU Machinery Regulation 2023/1230 in order to sell machinery across EU territories.

From Directive to Regulation: Why the Change?

One of the most important aspects of the EU Machinery Regulation 2023/1230 is that it will replace the Machinery Directive 2006/42/EC, changing the applicable policy framework from a directive to a regulation. In the EU legal hierarchy, a directive is a goal that each member state must achieve by writing its own national laws. This often leads to subtle differences in how safety is enforced internationally. The transition from directive to regulation means the policy is now a single law that applies across the entire EU. This shift eliminates legal fragmentation and ensures that a machine certified in one country meets the same standards in another.

Safety-Related Software Compliance

The 2023/1230 regulation was written specifically to address new challenges of Industry 4.0, such as the development of AI and emerging cybersecurity threats. As part of the new regulation, safety-related software is now recognised as an integral component, as opposed to an optional add-on at the manufacturer’s discretion. The regulation explicitly states that software critical to a machine’s safe operation must be protected against accidental or intentional corruption. This serves to protect manufacturers from new threats to health, safety, production, and profit caused by cyberattacks. The regulation’s requirements mean that manufacturers will need to monitor and document both legitimate and illegitimate interventions made to software for compliance purposes, and, in some cases, may even be required to complete a conformity assessment as part of CE marking.[3] This reflects a shift from the Machinery Directive 2006/42/EC, which did not directly address cybersecurity.

The Core Pillars of EU Machinery Regulation (2023/1230) Compliance

Once EU Machinery Regulation (2023/1230) is implemented in January 2027, manufacturers must address three primary pillars: Functional Safety, Cybersecurity, and Digital Documentation.

Enhanced Functional Safety

The Essential Health and Safety Requirements (EHSRs) in Annex III of Regulation (2023/1230) have been expanded to place greater emphasis on diagnostic coverage and fault tolerance.[4] This means that if a control system fails, the machine must transition to a safe state, therefore protecting the machine and outputs from further damage. For electronic components, this means a shift toward parts that support ISO 13849 (Performance Levels) and IEC 62061 (Safety Integrity Levels).[5] To comply with these standards, manufacturers can engineer components to include internal self-testing, redundancy, and the ability to report system health data to a central controller.

Mandatory Cybersecurity: Protection Against Corruption

Another significant shift in Section 1.1.9 of Annex III is the introduction of mandatory cybersecurity measures. This means manufacturers across EU member states are now legally required to enforce protection against corruption or hacking. Whether an attack is accidental or malicious, the regulation mandates that a machine’s safety functions cannot be compromised by remote access.

This security measure aligns with the Cyber Resilience Act (CRA), which mandates secure-by-design principles.[6] Manufacturers must ensure they enforce:

  • Hardware-based security can be achieved through practices such as Trusted Execution Environments (TEEs) and Secure Boot.
  • Life cycle support: Manufacturers must provide active support for at least five years (or the product’s estimated lifetime, whichever is longer) after the product is released to market. Further, documentation and security updates must be available for at least 10 years after introduction (or the remainder of the support period, whichever is longer).

Digitalisation and Technical Reporting

In contrast to the previous Directive (2006/42/EC), Regulation (2023/1230) embraces the digital age with digitised factory processes, allowing manufacturers to provide production resources using QR codes, web portals, PDFs, and other digital formats. However, in exchange for this flexibility, the technical file (known as the internal compliance dossier) must be more robust than previously required. This file includes detailed technical documentation, risk analysis, and evidence of cybersecurity testing and management.

The “Substantial Modification” Rule

Another crucial aspect of Regulation (2023/1230) is how it addresses older machines. If a manufacturer makes a substantial modification to an existing machine that creates or increases a risk, the machine may need to be re-certified to the 2027 standards. The market demand for secure small-form-factor components that can be integrated into existing cabinets is therefore expected to boom as a result of the new regulation.

Turning EU Machinery Regulation (2023/1230) into Profit: The Predictive Maintenance Strategy

A predictive maintenance (PdM) strategy is an approach to machinery maintenance that uses data from installed sensors to predict when and how equipment may fail. This approach includes the continuous monitoring of variables across machinery, from vibrations to pressure, to predict potential issues ahead of time.

Increasing Profitability

Unplanned downtime, including that due to machinery failures, results in estimated annual losses of £80 billion.[7] EU Machinery Regulation (2023/1230) may indirectly reduce these downtime losses by preventing sudden machinery failures through increased compliance with risk assessment requirements, prompting manufacturers to take action to prevent issues. This restructuring of the maintenance strategy will help prevent machinery downtime, therefore preventing potential profit loss.

How PdM Strategy Supports Compliance

PdM uses real-time data to forecast when a component will fail. By integrating PdM, manufacturers will achieve:

  • Residual risk reduction: Continuous monitoring identifies early failures before they become safety hazards.
  • Overall Equipment Effectiveness (OEE) optimisation: OEE increases when maintenance is scheduled during planned shutdowns rather than during emergency stops.
  • Sustainability: PdM has been shown to increase equipment lifespan by 20–25 percent, thereby potentially reducing the carbon footprint associated with equipment and part replacement.[8]

Component-Level Solutions for EU Machinery Regulation (2023/1230) Compliance

Mouser Electronics stocks solutions to help manufacturers meet these rigorous standards. To support system compliance with the EU Machinery Regulation (2023/1230) and an integrated PdM strategy, you may engage a sensor-to-cloud hardware chain.

Sensing for Diagnostics: Amphenol Advanced Sensors

To comply with the new monitoring requirements, sensors must be more than just on/off switches. They must provide granular digital data. The following sensors help enforce compliance:

Device

Use Case

Key Features

Amphenol Advanced Sensors NovaSensor NPI-19 Series

Media-isolated pressure sensors for hydraulic systems in heavy machinery

Digital I²C output; enables constant self-diagnostic checks; alerts controller if sensor drifts; suitable for high SIL ratings

Amphenol Advanced Sensors ZTPD-2210

Thermopile detector for non-contact temperature monitoring of moving parts

Detects overheating due to friction or electrical overload; documents temperature output; provides evidence of safe operation for technical files

Secure Edge Processing: NXP MCX Microcontrollers

A compliant machine’s edge controller must securely process sensor data, support AI-enabled PdM, and enforce real-time operation. NXP MCX-E-Series microcontrollers are well-suited for this role:

Device

Use Case

Key Features

NXP MCX E31 Series

Secure edge controller for sensor fusion, signal preprocessing, feature extraction, and lightweight AI inference supporting PdM

Robust 5V operation for high noise immunity in harsh industrial environments; integrated EdgeLock® security for a hardware-based root of trust; secure boot and key management to protect AI models and firmware from tampering; functional safety features suitable for safety-critical industrial systems

Secure Connectivity: Murata Wireless Modules

For machines to participate in a smart factory, they need wireless connectivity that meets the new regulations’ life cycle security mandate. Murata Wi-Fi and Wi-Fi+Bluetooth® modules support secure connectivity:

Device

Use Case

Key Features

Murata Wi-Fi and Wi-Fi+Bluetooth Modules

Wi-Fi 6 and Bluetooth Low Energy module designed for seamless integration with NXP i.MX platforms

Pre-certified for easy deployment; works directly with NXP microcontrollers

Reliable Power: Murata Power Solutions

A safety system is only as good as its power supply. EU Machinery Regulation (2023/1230) clarifies that systems must behave predictably and must not fail, even when the power supply fluctuates. The Murata NXJ1 isolated DC-DC converter supports this level of protection.

Device

Use Case

Key Features

Murata Power Solutions NXJ1T 1W DC-DC Converters

Provide reinforced isolation for industrial automation.

Feature proprietary block-coil technology delivering high isolation and excellent transient immunity. They also include built-in short-circuit protection and undervoltage lockout.

Designing Machinery for EU Regulation 2023/1230 Compliance

While the January 2027 deadline for EU Machinery Regulation (2023/1230) may seem distant, the complexity of these new requirements means that modification cycles within the industry must begin now.

By focusing on PdM, industries will strategise to invest in long-term compliance, but with potentially higher returns on investment due to the prevention of unplanned downtime.

With the right combination of Amphenol’s precision sensors, NXP’s secure processing, and Murata’s reliable connectivity, machinery will not only meet high safety standards but will also set new benchmarks for productivity. As a consequence of the new policy, we may see a fundamental shift toward a safer, more digital industrial world with a greater focus on profit protection and crime prevention.

   

Sources

[1]https://osha.europa.eu/no/legislation/directive/regulation-20231230eu-machinery
[2]https://osha.europa.eu/en/legislation/directives/directive-2006-42-ec-of-the-european-parliament-and-of-the-council
[3]https://europa.eu/youreurope/business/product-requirements/labels-markings/ce-marking/index_en.htm
[4]https://eur-lex.europa.eu/legal-content/EN/TXT/PDF/?uri=CELEX:32023R1230
[5]https://www.iso.org/obp/ui/#iso:std:iso:13849:-1:ed-3:v1:en; https://webstore.iec.ch/en/publication/59927
[6]https://eur-lex.europa.eu/legal-content/EN/TXT/HTML/?uri=OJ:L_202402847
[7]https://idsindata.co.uk/manufacturing-downtime-costs-and-forecasting/
[8]https://doi.org/10.36227/techrxiv.173532375.50630906/v1

 

Author Bio

Part of Mouser Electronics’ EMEA supplier marketing team, Simon Duggleby is a Senior Supplier Marketing Campaign Manager who brings an engineer’s perspective to supplier campaigns, drawing on his Electronic and Computer Systems Engineering background from Loughborough University.
At Mouser, he has supported Analog Devices’ One Tree Planted initiative in EMEA, and he also shares “tech for good” collaborations, including engineering that helps restore seagrass meadows and lidar-equipped drone work supporting whale conservation in Iceland.