Skip to main content

How Close is Wi-Fi 8 and What Can We Expect?

Image Source: Chanon/Stock.adobe.com; generated with AI

By Jean-Jacques DeLisle for Mouser

Published October 27, 2026

After the launch of Wi-Fi Certified 7 in early 2024, based on the IEEE 802.11be Extremely High Throughput (EHT) standard, attention soon shifted toward the next generation of wireless networking, Wi-Fi 8. Officially known as IEEE 802.11bn, the Wi-Fi 8 standard is still under development, with release expected in the 2027–2028 timeframe. Many aspects of the specification remain under discussion, as the IEEE 802.11 Task Group bn (TGbn) continues defining what the next generation of Wi-Fi should prioritize.

For decades, new Wi-Fi generations focused on increasing throughput with wider channels, higher-order modulation schemes, and expanded spectrum usage. Wi-Fi 8 appears to take a different direction: Instead of pursuing dramatic peak-speed increases, the standard is focused on improving reliability, reducing latency variation, minimizing packet loss, and maintaining stable performance in dense or interference-heavy environments. As wireless networking continues to move into industrial automation, real-time collaboration, augmented reality (AR) and virtual reality (VR), and artificial intelligence (AI)-driven systems, questions center more on how consistently it can perform than on how fast it can be.

This article discusses the current state of the Wi-Fi 8 specification, the priorities of the new standard, how it compares to Wi-Fi 7, and the new applications it may create.

How Wi-Fi 8 Builds on Wi-Fi 7’s Foundation

For several generations, Wi-Fi development mainly focused on increasing throughput via wider channels, higher-order modulation schemes, and more efficient use of spectrum. This is why Wi-Fi 7 was defined to support technologies such as 320MHz channel bandwidth, multi-link operation (MLO), 4096-QAM modulation, orthogonal frequency-division multiple access (OFDMA), and multiple resource units (MRUs).[1] Under ideal conditions, these technologies allow Wi-Fi 7 to theoretically achieve data rates approaching 46Gbps, compared to 9.6Gbps with Wi-Fi 6.[2]

In accordance with this trend, some may expect that Wi-Fi 8 will continue pushing toward wider channels, more spectrum, and more complex modulation schemes. However, the emerging IEEE 802.11bn standard seems to shift focus toward Ultra High Reliability (UHR). improving latency consistency, reducing packet loss, minimizing jitter, and maintaining stable performance in dense or interference-heavy environments.[3]

Throughput is no longer the primary limitation in many applications. Stadiums, factories, airports, apartment buildings, and enterprise campuses can all create congestion, overlapping networks, roaming interruptions, and fluctuating latency that affect real-time applications more than raw bandwidth limitations. Applications such as industrial automation, wireless backhaul, AR/VR collaboration, cloud gaming, and AI-assisted systems increasingly require fast, predictable networking performance. Even short bursts of latency variation or packet loss can disrupt workloads.

Some of the groundwork for this reliability-focused direction already appeared in Wi-Fi 7. Features such as MLO allow devices to coordinate traffic across multiple frequency bands simultaneously, helping reduce latency variation and improve link reliability. Likewise, MRUs and preamble puncturing improve spectral efficiency by allowing devices to better utilize partially occupied channels in cluttered RF environments.

Wi-Fi 8 is expected to expand on these concepts with more coordination, scheduling, and interference-management mechanisms designed to improve deterministic wireless behavior under real-world operating conditions (Table 1).

Table 1. Comparison of Wi-Fi 7 specifications and currently proposed Wi-Fi 8 specifications

Capability

Wi-Fi 7

Wi-Fi 8 (candidate, may change)

Availability

Current

2027–2028

Theoretical Maximum Data Rate

46Gbps (at least 30Gbps)

46Gbps (at least 30Gbps)

Supported Bands

2.4GHz, 5GHz, 6GHz

2.4GHz, 5GHz, 6GHz

Channel Bandwidth

≤320MHz

≤320MHz

Modulation

4096 QAM

4096 QAM

MLO

Yes

Yes, spectral efficiency improvements

Multiple Input, Multiple Output (MIMO)

Standard

Unequal Modulation per Spatial Stream

Mesh Networking

Standard

Multi-AP coordination enhanced

Power Efficiency

Standard

Additional Power Save Modes

Connectivity Range

Standard

Enhanced long range (ELR) and distributed-tone resource unit (dRU) techniques, especially on uplink

Distributed Resource Units (dRU)

NA

Yes

Coordinated Spatial Reuse (Co-SR)

NA

Yes

Coordinated Beamforming (Co-BF)

NA

Yes

Dynamic Sub-Channel Operation (DSO)

NA

Yes

Modulation and Coding Schemes (MCS)

Standard

MCS enhancements for better data rates over longer distances

Non-Primary Channel Access (NPCA)

NA

Yes

In-Device Coexistence (IDC)

NA

Yes

TXOP Preemption

NA

Yes

High-Priority EDCA (HIP EDCA)

NA

Yes

 

Wi-Fi 8 Improves Reliability and Coverage

Modern Wi-Fi networks must contend with limited performance due to client devices rather than the access point. Access points can transmit at high power levels, but regulatory transmit-power limits and battery considerations constrain smartphones, laptops, and Internet of Things (IoT) devices. Maintaining reliable uplink communication becomes more difficult as wireless networks become denser and users move farther from the access points.

Tackling user-device uplink constraints is also a potential target for Wi-Fi 8. Because wireless standards have transmit power constraints at certain frequencies due to regulation, simply increasing the uplink transmit power of a user device is not an option. However, it is possible to allow a device to transmit over a wider bandwidth and maximize power across the available channel. One approach, called distributed-tone resource units (dRU), could allow user devices to maintain uplink communication at greater distances and at higher noise thresholds.[4]

Current Wi-Fi access points (APs) essentially act as independent devices, even when they are designed to serve the same or overlapping areas. Wi-Fi 8 proposes enhanced coordination among APs, including coordinated beamforming, which would help ensure individual APs avoid interfering with each other. Other proposed methods for Wi-Fi 8 to avoid interference in multiple-AP environments (e.g., mesh Wi-Fi, enterprise installations) include time-scheduled transmissions (i.e., coordinated time-division multiple access (TDMA)), spatial reuse coordination, and seamless roaming through a no-interruption, make-before-break approach.

Some of these concepts appeared in Wi-Fi 7. Features such as MRUs and preamble puncturing allowed devices to better utilize fragmented or partially occupied channels in cluttered RF environments. Wi-Fi 8 is expected to build on this capability by enhancing access-point coordination, interference management, and roaming mechanisms that can improve performance in crowded wireless environments.[5]

Why Reliability Is Driving Wi-Fi 8 Development

Many modern wireless applications are becoming more sensitive to latency variation, packet loss, roaming interruptions, and inconsistent performance under congestion.

Wi-Fi 8 is expected to take the reliability, latency, and spectrum-utilization enhancement features of Wi-Fi 7 to the next level. The IEEE 802.11bn Ultra High Reliability Study Group, established in 2021, is responsible for developing the specifications for Wi-Fi 8. This group has acknowledged that current generations of Wi-Fi have theoretical peak throughputs that may exceed the requirements of real-world applications, while also causing intermittent connectivity issues, interference, and reduced performance due to protocol overhead in cluttered environments.

Increasingly, applications require more deterministic wireless behavior. Industrial automation systems, collaborative robotics, AR/VR platforms, wireless backhaul, cloud gaming, real-time video collaboration, and AI-assisted edge systems often need stable, low-latency communication rather than simply higher peak bandwidth.[6]

These requirements led the group to set a goal for Wi-Fi 8 to deliver a 25 percent improvement in throughput compared to Wi-Fi 7 (even under interference), a 25 percent reduction in latency distribution, and 25 percent lower MAC protocol data unit (MPDU) losses, especially during Basic Service Set (BSS) transitions.[7]

What Wi-Fi 8 Means for Enterprise, Industrial, and AI Applications

While Wi-Fi 8 is still years away from widespread deployment, many of the networking challenges that will drive the standard already exist. Dense wireless environments, overlapping networks, congestion, and latency-sensitive applications are becoming increasingly common across enterprise, industrial, and consumer systems.

As a result, many of the technologies introduced with Wi-Fi 7, such as MLO, improved spectrum utilization, coordinated access point behavior, and better interference management, are likely to remain important as wireless systems continue to support more real-time and reliability-sensitive workloads.

Engineers working on products for industrial automation, AR/VR, AI-assisted systems, robotics, or dense enterprise environments may need to consider latency consistency, roaming behavior, and coexistence, as well as traditional bandwidth metrics. While many details of IEEE 802.11bn are still evolving, the broader shift toward Ultra High Reliability already provides insight into where wireless networking priorities are heading next.

Conclusion

Many aspects of IEEE 802.11bn are still being developed, but the goals for Wi-Fi are becoming clearer. Wi-Fi 8 is expected to prioritize reliability, latency consistency, and improved performance in dense and interference-heavy environments rather than focusing on higher peak throughput. Features such as enhanced AP coordination, improved spectrum utilization, and deterministic networking mechanisms signal the need for more predictable wireless behavior across industrial, enterprise, and real-time applications.

Whether every proposed feature makes it into the final standard or not, Wi-Fi 8 represents a broader shift toward UHR as the next major priority in wireless networking.

   

Sources

[1]https://ieeexplore.ieee.org/document/11090080
[2]https://www.thenetworkdna.com/2026/02/wi-fi-6-vs-wi-fi-7-comparison.html
[3]https://doi.org/10.48550/arXiv.2507.09613
[4]https://www.asus.com/us/content/what-is-wifi8/
[5]https://www.qualcomm.com/news/onq/2025/07/wi-fi-8-advancing-wireless-through-ultra-high-reliability
[6]https://manufacturing-today.com/news/why-advanced-robotics-demand-reliable-deterministic-connectivity-by-amir-bushehri/
[7]https://www.ieee802.org/11/Reports/tgbn_update.htm

About the Author

Jean-Jacques (JJ) DeLisle attended the Rochester Institute of Technology, where he graduated with a BS and MS degree in Electrical Engineering. While studying, JJ pursued RF/microwave research, wrote for the university magazine, and was a member of the first improvisational comedy troupe @ RIT. Before completing his degree, JJ contracted as an IC layout and automated test design engineer for Synaptics Inc. After 6 years of original research--developing and characterizing intra-coaxial antennas and wireless sensor technology--JJ left RIT with several submitted technical papers and a U.S. patent. Further pursuing his career, JJ moved with his wife, Aalyia, to New York City. Here, he took on work as the Technical Engineering Editor for Microwaves & RF magazine. At the magazine, JJ learned how to merge his skills and passion for RF engineering and technical writing. In the next phase of JJ's career, he moved on to start his company, RFEMX, seeing a significant need in the industry for technically competent writers and objective industry experts. Progressing with that aim, JJ expanded his companies scope and vision and started Information Exchange Services (IXS).

Profile Photo of Jean-Jacques DeLisle