Skip to main content

Miniaturisation in Space: Designing Compact Yet Robust Components for the Final Frontier

The evolution of new launch systems has made space exploration more accessible than ever. Designers need low-profile connectors that will survive the harsh environments found in orbit. Find out how Harwin is developing connector solutions for the next generation of nanosatellites.

CubeSat nanosatellite orbiting Earth above cloud-covered surface

Image Source: NASA

By David Pike for Harwin

Published July 15, 2026

It is boom-time for the space industry. Around the globe, new research projects are being launched, and commercial companies are looking to the sky for new ventures. Recent years have seen consecutive records in the number of successful space launches, with this upward trend showing no signs of slowing.

Non-governmental applications for space flight have existed for many years. Communications, navigation and imaging have all been markets exploited by commercial ventures, but during this time, the mechanisms for launching equipment into space remained under the control of government institutions.

Making Spaceflight Affordable

Commercial space launch companies are powered by new technologies that have significantly reduced costs. At the height of NASA’s Space Shuttle program, the cost to launch equipment into Low Earth Orbit (LEO) was more than $50,000 per kilogram. In contrast, today’s Falcon 9 from SpaceX can perform the same task at an advertised cost of less than $3,000 per kilogram.[1]

The reduced costs have combined with other changes, including rideshare programs and dedicated small satellite launch systems. The practical result is that it is now feasible for smaller organisations to launch small satellites.

The market has thus been created for an entirely new generation of devices: nanosatellites. They are small and lightweight – often as little as a few kilograms. One example is the popular CubeSat concept, designed to a standardised form factor of 10cm cubes, which greatly simplifies their packing into launch systems.

Alongside reduced launch costs, designers are embracing the use of commercial-off-the-shelf systems (COTS). Using readily available components available on the commercial market further reduces the costs of space research and exploration. For the first time, it is even possible for schools and small businesses to create and launch their own satellites for pure scientific research as well as commercial applications. There are more than 4400 currently in orbit, and the number is growing every year.[2]

Advances in key technologies are contributing to this new generation of smaller satellites. Modern microelectronic systems are available in small and energy-efficient packages. These work in conjunction with miniaturised sensors, high-capacity battery systems, and high-speed communications to deliver powerful capabilities packed into small and light devices.

Nanosatellites are therefore masterpieces of compact design, with densely populated printed circuit boards delivering the greatest possible functionality within the limited space available. The key element that brings these systems together is the connector. Board-to-board connectors provide vital links between boards, while cables run up and down the outside of the board stack to carry power and data to all components.

Connectors for Extreme Conditions

Despite the capabilities that can be packed into these small devices, designers of nanosatellites must also contend with one of the harshest environments experienced by any industry. The vacuum of space, combined with extreme temperatures and long-term exposure to radiation, makes designing satellites a unique challenge.

Without the protection of the Earth’s atmosphere, any object in space will receive the full force of the sun’s radiation. In locations exposed to direct sunlight, temperatures can rapidly rise to dangerous levels, while areas that remain in shadow become very cold. The materials from which components are constructed must be chosen with great care to deliver a wide operating temperature range.

The absence of atmospheric pressure also causes materials to behave in unusual ways. In vacuum conditions, some materials release gases that are trapped during their manufacture. This is a process known as outgassing, and is a common problem when plastic is exposed to a vacuum during spaceflight. Gas that is released can condense onto cold surfaces, including the sensors of scientific equipment, severely compromising their functionality.

Reliability

Satellites must function for long periods whilst remaining far beyond the possibility of repair. Connectors designed for spaceflight, therefore, need to provide long-term reliability and resistance to the rigours of launch whilst remaining as light as possible.

Alongside the need for mechanical reliability, satellites must be designed for long-term missions. During their mission, power management becomes a major concern, and space vehicles must be designed to ensure the greatest possible duration. Operating within a strict power budget, any component that introduces unwanted electrical resistance can put the mission at risk.

Gecko from Harwin

The Gecko connector series from Harwin is ideally suited for the three-dimensional puzzle that designers face when creating the latest generation of nanosatellites. They combine compact size with high performance and reliability, enabling them to withstand the conditions encountered in spaceflight applications.

At the heart of the Gecko connector is its machined contact. Using a 1.25mm pitch, these miniature contacts are highly durable, capable of over 1000 operations while resisting the shocks and vibration associated with space launch. Their low contact resistance minimises losses and enables efficient power and signal transmission throughout the satellite.

Figure 1: Gecko connector contacts size comparison. (Source: Harwin)

In the limited space available inside the satellite, the Gecko-MT (“Mixed Technology”) series combines the 1.25mm-pitch signal contacts with larger power contacts fitted within the same housing that can carry up to 10 Amps per circuit. With this mixed signal and power capability, Gecko-MT delivers a flexible and low-profile solution for areas where PCB real estate is at a premium.

Other features that make them ideal for spaceflight applications include the use of high-performance materials. The glass-filled thermoplastic insulator delivers an operating temperature range of -65°C to +150°C. It is also a material with low outgassing properties, making an ideal solution for exposure to the vacuum of space. The Gecko series can also be protected against electromagnetic interference (EMI) with the use of machined aluminium backshells.

Figure 2: The Gecko MT group. (Source: Harwin)

Conclusion

The growing commercialisation of space offers small organisations the opportunity to create their own satellites. However, despite this commercialisation, the tough conditions of spaceflight require designers to pay close attention to the components they use.

Harwin manufactures connectors designed especially for high-reliability applications. The Gecko and Gecko-MT series provide ideal solutions for designers creating the next generation of nanosatellites and the further exploration of space.

 

The “Miniaturisation in Space: Designing Compact Yet Robust Components for the Final Frontier” blog was previously published by Wevolver and is republished here with permission.

   

Sources

[1]https://ntrs.nasa.gov/citations/20200001093
[2]https://www.nanosats.eu/

About the Author

Harwin is a manufacturer of High Reliability Interconnects suitable for harsh environments and are able to withstand extreme vibration, shock and temperature. Datamate, Gecko and M300 product lines have a proven history in Military, Aerospace and other safety critical markets. Other board level solutions include EMC Shielding products which increase reliability, flexibility and cost savings through the process of automated placement. Industry standard connectors and PCB hardware are also available from Harwin for commercial applications.