Perovskite-Silicon Tandem Solar Cells for High-Efficiency Energy

Image Source: DigitalSpace/Stock.adobe.com; generated with AI
By Mouser Technical Content Staff
Published May 28, 2026
Global energy demands mandate scalable, efficient generation technologies to replace aging legacy infrastructure. Traditional power plants require years of construction and massive capital investments before generating a single watt of power. Photovoltaic (PV) energy provides a rapidly deployable alternative, yet fundamental material constraints hinder absolute generation capacity. Recent breakthroughs in materials science have introduced programmable crystalline structures that can stack directly onto legacy panels, fundamentally rewriting the rules for capturing solar energy.
To understand the trajectory of this technology, we examine insights from Scott Wharton, CEO of Tandem PV, who recently discussed these materials science breakthroughs on Mouser Electronics’ The Tech Between Us podcast. This article explores the physical constraints of traditional silicon solar cells, examines the optoelectronic properties of perovskite crystals, and details the efficiency gains of stacked (i.e., tandem) architectures, which can help enable higher-performance, flexible, indoor, and grid-scale energy harvesting for next-generation renewable power systems.
The Physical Constraints of Silicon Solar Cells
Silicon dominates the solar industry due to highly standardized manufacturing processes and abundant raw materials. Fundamental physical laws prevent standard silicon from converting the entire solar spectrum into electrical current, but utility-scale silicon panels average around 20 percent efficiency in the field.[1] Single-junction crystalline silicon cells have a theoretical power conversion efficiency (PCE) limit of 29.4 percent.[2] However, real-world field implementations suffer from inescapable thermalization and recombination losses, bringing practical maximum limits closer to 26 percent.[3] Surpassing this hard physical ceiling requires multiple absorber materials with distinct band gaps to capture different segments of the incoming light spectrum.
The Material Science of Perovskite Crystals
To surpass standard silicon’s physical ceiling, engineers are turning to a material capable of capturing the light spectrum that silicon misses: perovskite. Perovskite has a highly specific crystal structure composed of three distinct elements, offering tunable optoelectronic properties. Engineers synthesize these crystals entirely in the laboratory, eliminating the need to mine rare-earth minerals. The manufacturing process converts the raw perovskite into a printable semiconductor ink, film, or powder, enabling engineers to create deposition layers as thin as 100nm. This extreme thinness represents an active layer 200 times thinner than conventional silicon wafers. Fabricating these ultrathin layers requires only 10 percent of the energy consumed in standard silicon semiconductor production, thereby reducing total lifecycle emissions while driving down unit costs.[4]
Tandem Architecture: Multiplying Efficiency
Because perovskite’s optoelectronic properties are tunable, engineers can stack a specialized perovskite layer directly on top of traditional silicon, creating a multi-junction architecture capable of absorbing a drastically wider band of solar radiation. Stacking different semiconductor materials creates a multi-junction architecture capable of absorbing a drastically wider band of solar radiation. Capitalizing on this architecture, tandem PV arrays combine an ultrathin perovskite top layer with an off-the-shelf silicon bottom layer. The perovskite layer intentionally allows 40 percent of incoming light to pass through to the underlying silicon. This enables the bottom layer to convert the remaining spectrum into power, effectively multiplying the total energy harvested. Current mechanical stack iterations from Tandem PV achieve 28 percent efficiency, outperforming standalone silicon by 30 percent. The theoretical limit for this specific perovskite-silicon tandem structure is near 45 percent, though experimental triple-stacked material variants might eventually push theoretical limits up to 50 percent.[5]
Flexible Substrates and Novel Form Factors
The ink-like nature of perovskite materials enables physical applications that are impossible with rigid, brittle silicon wafers. Manufacturers can deposit perovskite films directly onto flexible plastics, metallic foils, and fabrics (Figure 1). Consumer technology companies are currently experimenting with applying these energy-generating inks to passive surfaces, such as umbrellas, vehicle paint, and outdoor clothing.

Figure 1: An ultrathin perovskite solar cell deposited onto a flexible plastic substrate demonstrating extreme bendability and mechanical resilience. (Source: DigitalSpace/stock.adobe.com; generated with AI)
Unlike rigid glass panels, these flexible substrates maintain high performance under extreme physical strain. For example, in one study, devices subjected to a 30 percent compressive strain retained 83 percent of their initial outdoor efficiency.[6] This flexibility allows engineers to convert passive surfaces into active power generators without altering the underlying object’s aerodynamic or physical design.
Indoor Energy-Harvesting Capabilities
Indoor environments pose unique spectral challenges that render standard silicon photovoltaics ineffective. Silicon cells require intense, broad-spectrum outdoor light to function optimally, rendering them unsuitable for low-power ambient electronics and Internet of Things (IoT) hardware. Perovskite structures, however, demonstrate exceptional performance under cooler indoor lighting conditions. A 2024 laboratory test achieved a 34 percent PCE under illumination from an 870lx white light-emitting diode (LED).[7] This means that extracting energy from ambient office lighting could mitigate the parasitic power drain caused by idle wall chargers and permanently connected IoT devices. As a result, high-efficiency indoor harvesting would enable developers to design self-sustaining wireless sensor networks that don’t require frequent manual battery replacements.
Encapsulation and Degradation Mitigation
Environmental exposure threatens the chemical stability of these crystalline structures. Moisture is particularly damaging, rapidly degrading perovskite solar cells when relative humidity exceeds 70 percent.[8]
Engineers deploy robust encapsulation techniques to block moisture ingress and permanently trap internal elements. Standard utility-scale panels use thick glass on both sides of the active layer to create a highly durable hermetic seal. This sealing process prevents lead leakage during extreme weather events or physical damage. While the active layer contains trace amounts of lead, the robust hermetic seal prevents it from escaping. Hermetic sealing protocols simultaneously prevent oxidation and stabilize internal ion migration, drastically extending operational field lifetimes.[9]
Grid Integration and Deployment Scale
Utility networks demand standardized, reliable generation hardware to rapidly replace legacy fossil-fuel infrastructure. Solar deployments dominate new grid additions because standard panels arrive off the shelf and require minimal installation time compared to natural gas facilities. Global solar installations reached 600GW in 2024, with China alone deploying over 350GW.[10] In the United States, solar, wind, and battery storage accounted for 90 percent of all new energy additions that year.[11] Component costs for battery storage have plummeted by 70 percent over the last decade, allowing grid operators to store excess daytime generation for reliable evening distribution.[12]
“I think we think of solar as only being on someone’s roof, but in the US, I think less than about 10 percent of the solar is deployed as residential,” Wharton observes. “More than 80 percent of it is actually the solar farms that you see when you are driving along the highway” (Figure 2).

Figure 2: Utility-scale PV arrays provide hundreds of gigawatts of power to modern electrical grids when paired with high-capacity battery storage systems. (Source: TechNova Graphics; generated with AI)
Conclusion
As the solar industry hits the physical efficiency limits of traditional silicon, understanding the latest breakthroughs in perovskite tandem architectures is critical to unlocking the flexible, highly efficient, and scalable energy capture required to stabilize modern power grids. Silicon’s conversion efficiency has a hard limit of just under 30 percent. Perovskite technology bypasses these legacy limits, offering a printable, highly efficient material that pairs natively with existing silicon substrates to boost output. Flexible deployment options expand generation into indoor spaces and curved surfaces, while rigorous hermetic encapsulation addresses moisture-related degradation and toxicity concerns. Unprecedented global installation rates highlight the rapid transition toward decentralized, renewable generation, providing the grid with constant, reliable power day and night.
Sources
[1]https://css.umich.edu/publications/factsheets/energy/solar-pv-energy-factsheet
[2]https://ieeexplore.ieee.org/document/6557081
[3]https://resources.mouser.com/eit-reduce-reuse-reimagine-tech/eit2025ttbu-episode2-en
[4]https://resources.mouser.com/eit-reduce-reuse-reimagine-tech/ttbu-rrrtech-1
[5]https://resources.mouser.com/eit-reduce-reuse-reimagine-tech/eit2025ttbu-episode2-en
[6]https://doi.org/10.1021/acsaem.3c02581
[7]https://doi.org/10.1021/acsami.4c14736
[8]https://doi.org/10.1063/5.0197154
[9]https://doi.org/10.1021/acsami.5c02993
[10]https://iea-pvps.org/wp-content/uploads/2025/04/Snapshot-of-Global-PV-Markets_2025.pdf
[11]https://www.wri.org/insights/clean-energy-progress-united-states
[12]https://resources.mouser.com/eit-reduce-reuse-reimagine-tech/ttbu-rrrtech-1