Skip to main content

Why Counter-Drone Technology Is Now Mission-Critical

Image Source: miss irine/stock.adobe.com; generated with AI

By Mouser Technical Content Staff

Published February 17, 2026

Airspace management has changed significantly. Today, small drones and other uncrewed aerial systems (UASs) can influence how ground crews respond to possible threats without ever involving crewed combat aircraft. As a result, operational realities have shifted, and organizations must protect people and assets differently.

UASs are showing up in more roles than could have been anticipated even a decade ago. Small quadcopters are used for reconnaissance and targeting, and one-way uncrewed aircraft are increasingly used for precision, one-time missions.

The problem is that most traditional airspace protection systems were not designed for small, low-altitude objects. Radar systems designed for high-speed flight profiles can struggle to detect slower, low-altitude objects that have very small or weak radar signatures.

Cost is also a consideration. Using expensive physical countermeasures against small drones can be difficult to justify when the interceptor can cost more than the target. These gaps have necessitated new systems that can specifically address this risk category.

To address these challenges, designers must understand the risk landscape and the technologies used to mitigate it. Current counter-UAS efforts include a range of strategies, such as detecting and tracking drones and then disrupting navigation and communications (or otherwise rendering them non-operational) using electronic or energy-based methods. Global Positioning System (GPS) spoofing and radio frequency (RF) jamming are already part of today’s counter-UAS strategies. High-power microwave and energy-focused systems are increasingly appearing in real-world pilot programs and assessments rather than just in test programs.

No single technology is enough on its own. Systems that rely on layered sensing and a mix of countermeasures tend to be more effective than those built around a single technique, especially when protecting forces and critical infrastructure in the real world.

How the UAS Risk Is Changing

Uncrewed aircraft in high-risk environments range from small commercial quadcopters to purpose-built systems.[1] At one end of the spectrum are drones that can be purchased off the shelf and adapted quickly. These types of UASs are often used for observation and cueing, and some may carry small payloads. From a distance, it is hard to distinguish them from civilian drones, which can complicate response decisions. At the other end of the drone spectrum are more robust, purpose-built UASs designed for extended operations and harsh conditions. They use stronger communication links and contain navigation systems that keep operating even when signals are disrupted.

Even small drones can affect ground defense, as they are often used to observe points of interest and adjust indirect effects in near real time, which can change the outcome and response. Even if the drone is neutralized, the information it provided while active can still be decisive.

At scale, protection teams may face multiple platforms that arrive rapidly from different directions. Systems that work well against isolated targets may struggle as the volume of UASs increases.

Many platforms still rely on satellite navigation and radio links, which are vulnerable to disruption. But those same vulnerabilities push operators to adapt. Encrypted communications and frequency hopping are becoming more common avoidance tactics. This results in a continuously evolving high-risk environment, making it challenging to design defenses around a single predictable pattern. 

All of this presents challenges to defense teams. Drones are harder to see and often used in ways they weren’t originally designed for. That poses both operational and design challenges for engineers developing counter-UAS technology.

Most systems rely on a combination of detection methods, with each compensating for the limitations of the others.

Detection and Tracking Technologies

Detecting small drones is more challenging than most legacy systems were designed for. Since small drones fly low and blend into background clutter, modern counter-drone systems rarely rely on a single sensor. Most approaches layer multiple detection methods.[2]

Radar plays a significant role but has had to evolve. Traditional air-defense radars were designed for aircraft and high-altitude, high-radar-cross-section (RCS) objects, not for tiny platforms just above the tree line. Newer short-range radars are being designed specifically to focus on low-altitude airspace and apply more advanced signal processing so small drones don’t disappear. In many systems, radar offers the first indication that something may be present, allowing other technologies to take over.

RF sensing has become increasingly important, especially against commercial drones that rely on known communication protocols.[3] Passive RF systems continuously monitor the electromagnetic spectrum for control signals, telemetry, and video links, which makes them harder to detect and useful in environments where operators don’t want the systems to emit energy. In some cases, RF analysis can go beyond drone detection and help pinpoint the operator’s location.

Once a potential target has been detected, the next step is typically visual confirmation, which often involves electro-optical cameras and infrared sensors. This method is critical in environments where civilian drones may be present.[4]

Acoustic sensing plays a minor role but still appears in some systems. Sensors can detect the sound of small motors and propellers in certain environments, especially at short range. While acoustic sensing alone is insufficient, combining it with other detection methods can provide an additional data point for defenders.[5]

Since no single technology detects everything clearly all the time, sensor fusion ties everything together. With combined radar, RF, camera, and acoustic data, the overall picture becomes more reliable. This layered approach is becoming more common and indicates a shift away from standalone counter-drone systems.

Mitigation Techniques

Detecting the drone is the first step, but then the defense team must determine its response. Many of today’s counter-drone systems rely initially on electronic or energy-based approaches. These are methods that disrupt and disable electronics rather than physically damaging them. These methods scale better and reduce the risk of collateral effects compared to solely kinetic responses.

One of the most common areas of focus is navigation, as many drones depend on it for positioning, stabilization, and waypoint following. When navigation signals are disrupted, the drone can lose its ability to function properly. GPS jamming overwhelms the receiver with noise, preventing it from locking onto a usable signal.[6] Spoofing is a more subtle tactic that introduces false navigation data, leading the drone to misinterpret its location. In some situations, this can cause the aircraft to drift off course or descend. However, this strategy proves less effective if the drone uses more advanced navigation techniques, encrypted signals, or multiple satellite constellations.

Communication links are another common target. RF jamming disrupts the connection between the drone and the operator by interfering with command signals or video feeds. When those links fail, many drones default to predefined behaviors, such as hovering, landing, or attempting to return to the launch point.[7] RF jamming is widely used because it can be effective against many commercial platforms, but it must be performed carefully. In crowded electromagnetic environments, poorly controlled jamming can interfere with other systems (e.g., civilian communications), so precision and control are critical in real deployments.

High-power microwave (HPM) systems take a different approach. Instead of disrupting signals, they use short bursts of electromagnetic energy that can disrupt or degrade onboard electronics. This is an appealing tactic in scenarios with multiple drones because a single response can affect more than one target.[8] The trade-off is that the systems can have a broader unintended impact on nearby equipment, so they must be carefully managed.

High-energy laser systems are gaining attention for their precision in impairing specific subsystems. (e.g., sensors, propulsion) to impair function. Because of this precision, these systems are well-suited for defending fixed sites such as bases and critical infrastructure.[9] Their limitations are practical; they require a clear line of sight, sufficient power, and ideal atmospheric conditions. However, rain and dust can reduce effectiveness, which is why they are often part of a layered defense system rather than a standalone solution.

Physical options, such as intercept devices, capture mechanisms, or intercepting UASs, may be used when other methods are ineffective.[10]

Operational Use and Integration

Counter-drone systems are appearing in more places and in more forms than they were even a few years ago. Some are mounted on vehicles and move with units in the field, while others are fixed around bases and infrastructure. These tools are no longer treated as standalone add-ons. Instead, they are integrated into existing airspace protection, electromagnetic spectrum operations, and C2 systems, so information can be shared quickly.

Timing is imperative in these environments. Drones can appear and depart quickly, leaving a short response window for detection and action. As a result, system designers must focus on how sensors, software, and countermeasures interact. Many platforms use automated alerts and cueing to help operators keep up with activity, especially when multiple drones are in use. This functionality helps keep people from having to piece together information manually when under time pressure.

Day-to-day operations are also evolving. Units must consider how their own emissions appear to others and how different teams coordinate response. These tools are now part of routine operations rather than isolated capabilities.

System Constraints and Design Considerations

Counter-drone technology has advanced quickly, but it still operates within real-world constraints. It is difficult to consistently detect small UASs, particularly in dense urban environments where buildings and background signals generate significant noise. Because of this, many teams focus less on perfect detection and more on building systems that can adapt to imperfect information.

As drones gain onboard autonomy, encrypted communications, and frequency agility, older electronic techniques no longer work as reliably as they once did. That is one of the reasons for a layered approach, rather than reliance on any single method.

There are also practical boundaries beyond engineering. Outside of active high-risk regions, counter-drone systems must operate within legal and regulatory frameworks, especially when civilian communications and aviation systems are nearby. These frameworks dictate how systems are designed and deployed, and have pushed many teams toward more precise, controlled tools instead of broad, blunt responses.

Rather than being seen as obstacles, these constraints are shaping the direction of the technology. They are part of why flexibility, modular design, and system-level thinking have become central to modern counter-drone development.

Conclusion

As UASs and their risks continue to evolve, counter-drone capabilities are now standard for protecting people, operations, and infrastructure. Effective mitigation is a combination of methods that use detection, electronic techniques, and (selectively) energy-based tools. Future progress is likely to come from steady improvements in sensing, integration, and system design as engineers adapt to how these platforms are used.

 

Sources

[1]https://www.washingtoninstitute.org/policy-analysis/nato-counterterrorism-trends-current-and-future-threats
[2]https://www.cnas.org/publications/reports/countering-the-swarm
[3]https://www.quickset.com/cuas-counter-unmanned-aircraft-systems/
[4]https://www.defenseadvancement.com/feature/enhancing-cuas-with-advanced-ir-thermal-imaging-lenses/
[5]https://www.mindfoundry.ai/blog/acoustic-intelligence-for-counter-uas
[6]https://www.uavnavigation.com/company/blog/jamming-and-spoofing-two-threats-your-uas-gnc-system
[7]https://cuashub.com/en/glossary/rf-jamming/
[8]https://www.army-technology.com/projects/leonidas-high-power-microwave-hpm-system-usa/
[9]https://cuashub.com/en/content/aerovironment-delivers-their-first-high-energy-laser-counter-uas-systems-to-u-s-army/
[10]https://www.defenseadvancement.com/news/advanced-kinetic-cuas-system-launched/

About the Author

Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.

Profile Photo of Mouser Technical Content Staff