LoRa Flipbooks

How to Deploy a LoRa®-based Network for your IoT Application

Issue link: https://resources.mouser.com/i/1300213

Contents of this Issue

Navigation

Page 6 of 17

White Paper — How to Deploy a LoRa®-based Network for your IoT Application Page 7 of 8 The Sensor Nodes The sensor nodes of the Dots on a Map solution are where all of the data sampling takes place. As such, each node contains a wide array of sensors so that many use-cases can be addressed with a single hardware design. The RX231 is the central component of the sensor end node. All of the sensors are connected to the RX231, the majority via I2C interfaces, while the others are connected through SPI and UART interfaces. The RX231 is responsible for sampling all of these sensors and then communicating the sensor data to the gateway through the LoRa radio frequency. Refer to the following block diagram for more detail. Each sensor node is designed to operate both indoors and outdoors using an enclosure that has ventilation and moisture protection. A standard SMA connector is exposed for attaching a LoRa antenna, and both micro-USB and banana plug options are exposed for providing power to the unit.

Articles in this issue

view archives of LoRa Flipbooks - How to Deploy a LoRa®-based Network for your IoT Application