Supplier eBooks

Qorvo - Next-Gen Wi-Fi Applications and Solutions

Issue link: https://resources.mouser.com/i/1313794

Contents of this Issue

Navigation

Page 25 of 27

26 Designing for Next Gen Wi-Fi Applications Fighting for wireless bandwidth, especially in tightly packed device-filled environments such as stadiums and rallies is sketchy at best. Over-subscribed carriers are part of the problem. They just cannot provide enough raw data to so many people in real time. But competing in the same space as some cellular bandwiths is Wi-Fi, ZigBee™, Bluetooth®, DECT, HAL, and several other protocols we may be aware of–all sharing RF space, all using different modulation schemes, channel widths, channel spacings, and frequency-hopping algorithms. As next-generation services and devices emerge, more frequencies, bandwidth, coexistence, and interference immunity are needed. This means claiming more of the spectrum that was lost using older technologies. Read on to learn how Bulk Acoustic Wave (BAW) technology offers a promising solution to maximize spectrum utilization by supporting more precision filtering to recover stronger, more reliable signals with greater noise immunity. Maximizing Spectrum Utilization Spectrum utilization is the key, and while the move from 3G to 4G increased from 5 bands to 20 bands, soon 40 4G bands will be up for grabs, all trying to recover clean signals from a world of muddying interference. In other words, reaching deep into a turbulent pool of RF, more precision filtering is needed to recover stronger and more reliable signals with improved noise immunity. And with handheld devices that feature multi-protocol transceivers that can operate simultaneously, the need for 40 filters is not uncommon. Even within home settings, Wi-Fi routers suffer and end-point devices fall victim here as well. We need more reliable data, more throughput, fewer retries, more effective range, more simultaneous channels, and so on. QPQ1909 Wi-Fi edgeBoost ™ BAW Filter QPF4550 5GHz Wi-Fi 6 Front End Modules • Low insertion loss in Wi-Fi channels 1 to 14 • Extended temperature performance from 0 to +90°C • High power handling to +30dBm averaged input power • Optimized for +5V Operation • 13.5dB Rx Gain & 8dB Bypass Loss • POUT = +24.5dBm MCS0 HT20 Spectral Mask Compliance LEARN MORE > LEARN MORE > Next-generation wireless: Bulk Acoustic Wave filters are small, handle high power, feature sharp band edges, and low insertion loss. https://bit.ly/2Dq1np7 https://bit.ly/33sMdKV

Articles in this issue

Links on this page

view archives of Supplier eBooks - Qorvo - Next-Gen Wi-Fi Applications and Solutions