Supplier eBooks

Qorvo - Harnessing the Power of 5G

Issue link: https://resources.mouser.com/i/1313800

Contents of this Issue

Navigation

Page 14 of 29

| 15 | Comparing 4G and 5G The figure above provides a comparison of the performance characteristics and technical specifications of 4G and 5G technology. The following table summarizes the major differences between 4G and 5G technology. Currently, use cases are being defined, new radio access technologies are being developed, and carrier field trials are being conducted. The Third Generation Partnership Project (3GPP) standards body is harmonizing and globalizing these new ideas into a unified specification. By adopting LTE Advanced (LTE-A), carriers are making considerable progress toward the speed goals for 5G (see graph below), but more work is required. 4G (Today, Before Further Developments) 5G Latency 10ms Less than 1ms Peak data rates 1Gbps 20Gbps Number of mobile connections 8 billion (2016) 11 billion (2021) Channel bandwidth 20MHz 200kHz (for Cat-NB1 IoT) 100MHz below 6GHz 400MHz above 6GHz Frequency band 600MHz to 5.925GHz 600MHz–mmWave (for example, 28GHz, 39GHz, and onward to 80GHz Uplink waveform Single-carrier frequency division multiple access (SC-FDMA) Option for cyclic prefix orthogonal frequency-division multiplexing (CP-OFDM) User Equipment (UE) transmitted power +23 decibel- milliwatts (dBm) except 2.5GHz time-division duplexing (TDD) Band 41 where +26dBm, HPUE is allowed IoT has a lower power-class option at +20dBm +26dBm for less than 6GHz 5G bands at and above 2.5GHz Downlink Speeds by Technical Generation The Path to 5G Deployment Enhancing the mobile wireless experience is a step-by- step pathway for carriers, requiring further expansion and development of 4G and moving toward LTE-A technologies. Carriers are currently in the midst of developing software-defined networks (SDNs), heterogeneous networks (HetNets), and low power networks. Finally, in 2019 and beyond, global 5G rollouts and initial commercial releases will begin (see figure to the below). Want more details about what's to come with 5G? Download a copy of our latest e-book, 5G RF For Dummies ® . – Excerpted with permission from John Wiley & Sons, Inc., from 5G RF For Dummies.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Qorvo - Harnessing the Power of 5G