5G Document Folder

The Future of 5G

Issue link: https://resources.mouser.com/i/1315957

Contents of this Issue

Navigation

Page 44 of 51

| 44 have more complex requirements involving vehicle-to-anything (V2X) communications, which include low- latency control functions and high bandwidth requirements. Vehicles offer flexibility for embedding antenna arrays into the bodies of the vehicles themselves. Cell Phones Cell phones are already packed with antennas, so adding antennas to support the full range of 5G frequencies will be a challenge. These phones also have limited real estate, but they will need MIMO antennas for high-level performance and antennas located on the phones' edges and corners that support beamforming, specifically to compensate for objects that block millimeter waves (mmWaves), like a user's hand. The Challenges of 5G Antenna Designs 5G antennas have a key role to play in making 5G communications work, but they present engineering challenges. Antenna designers typically begin with antenna simulation software that, given certain assumptions, can project signal fields. But, this is only a first step. A significant challenge in 5G antenna designs is antenna testing. 5G antennas are not static, omnidirectional devices. They are active, and they beam their transmissions to specific devices. Putting a 5G antenna in a test room and applying a static test does not show how it will perform when it is simultaneously communicating with a thousand moving devices in a noisy RF environment. Most antenna designers are not sure of the most effective means to test or validate performance for devices that use mMIMO arrays. Testing methods will likely involve scenario-based automated testing. 5G antenna designs are still very much a work in progress. The initial phase of the 5G deployment is just beginning, and it will involve installing low-frequency 5G to work in collaboration with 4G LTE. This is the testbed for future deployments requiring more complex antenna designs. mouser.com/nxp-5g-mmimo mouser.com/johnson-cinch-5g-connectors Johnson / Cinch Connectivity Solutions Connectors for 5G Applications NXP 5G mMIMO High-Efficiency Power Amplifier Modules

Articles in this issue

Links on this page

view archives of 5G Document Folder - The Future of 5G