Issue link: https://resources.mouser.com/i/1315957
| 14 multiplexing of different kinds of subframes, and they support blank subframes to accommodate undefined future services. Self-contained subframes can also contain beamforming data specific to a transmission, which supports multiple-input, multiple-output (MIMO) antenna transmissions and reduces interference. • Device-centric mobility. In LTE networks, receiving devices measure reference signals that base stations transmit to decide where to connect. Base stations transmit reference signals continuously, regardless of the presence of a receiving device—which requires processing overhead on the receiving device and excess power consumption by the transmitting equipment. In 5G transmissions, receiving devices transmit a reference signal when they need a network connection, and this reference signal triggers communication and handoff activities using appropriate transmitting equipment. This arrangement reduces power consumption and the number of reference signal broadcasts. • New cell architectures and antenna designs. To support larger numbers of connected devices, uninterrupted communications, and shorter operational ranges available from high-frequency bands, 5G will require denser cell architectures than are found in 4G LTE networks. Typical deployments could include a mix of macro-cells operating in low frequencies for wide outdoor coverage, small cells operating indoors and outdoors in mid-frequency ranges, and micro- cells (room sized) operating primarily indoors at millimeter wavelength frequencies. Beamforming techniques using massive MIMO (mMIMO) antenna arrays will provide uninterrupted coverage and much higher transmission efficiencies than 4G LTE produces with previous MIMO variations. 5G antenna designs will also produce more signal processing at the antennas to manage mobile device handoffs between cells. 5G Core Virtualizes 4G Evolved Packet Core Network Architecture To meet 5G performance specifications, especially as they relate to use case flexibility, scalability, and reliability, the 5G Core network has been redesigned from the ground up in a way that completely supplants the 4G Evolved Packet Core (EPC). Whereas 4G EPC relied on physical network elements, 5G Core is a cloud-native virtualized architecture that uses multi-access edge computing to deliver network functions as services to a network's edge. Key features and capabilities of the 5G Core architecture include: • Separate control plane and user plane functions. This separation and reallocation of functions previously performed by EPC service and packet gateways enable a redistribution of packet processing functions to a network's edge. The result is better traffic management and scalability. • Redesign of session management functions. Mobility management and session management are now performed by different network elements, and new identity and authentication functions have been added. All this improves session management to deliver uninterrupted service in various operational scenarios—for example, as user equipment is moving through a small cell network or at high speeds. These session management enhancements create a reliable service flow in complex environments that contain dense IoT arrays and user equipment with diverse data formats. • Network slicing. This technology enables 5G to offer a "slice" of the network as a dedicated service for a particular use case, customer, or industry. User equipment can simultaneously access multiple network slices. A network slice maintains all necessary functionality and quality across domains and technologies to efficiently allocate available resources for each use case. New Applications and Business Cases Possible with 5G The 5G standard enables a range of simultaneous communications that are highly reliable and optimized for use case performance and power consumption. This standard opens the door to a host of new smart services and partnerships that could not previously be accommodated on monolithic 4G networks. Use Case Possibilities: Life in a 5G World To illustrate some of the possibilities in a 5G world, consider a simple example of an architect's commute to work one morning in her autonomous vehicle (AV). It happens that she has scheduled a conference call to take place during her commute because this was the only time her clients in Spain and her supplier in Singapore could meet. [ C O N T ' D O N N E X T P A G E ]