Supplier eBooks

Analog Devices - Industry 4.0 and Beyond

Issue link: https://resources.mouser.com/i/1437657

Contents of this Issue

Navigation

Page 24 of 37

25 Industry 4.0 and Beyond | ADI This calculation assumes no other traffic on the network or that the network is managed to enable priority access for time- sensitive traffic. It is also somewhat protocol dependent, with slight variations in the calculation being introduced depending on the exact Industrial Ethernet protocol used. Referring back to Figure 2, in a machine system with cycle times down to 50µs to 100µs, the frame transmission to the furthest node can take up to almost 50 percent of the cycle, reducing the time available to update the motor control and motion control algorithm calculations for the next cycle. Minimizing this transmission time is important for performance optimization, as it allows longer and more complex control calculations. Given that delays associated with data on the wire are fixed and related to the bit rate, utilizing low latency components, such as the ADIN1200 PHY and the fi do5000 embedded switch, is key to performance optimization, especially as node count increases (for example, 12-axis CNC machine) and cycle times reduce. Moving to gigabit Ethernet dramatically reduces the impact of bandwidth delay but increases the proportion of overall latency introduced by the switch and PHY components. For example, a 12-axis CNC machine on a gigabit network will have a network transmission delay of approximately 7.5µs. The bandwidth element of this is negligible, and it makes little difference whether minimum or maximum Ethernet frame sizes are used. The network delay is split approximately equally between the PHYs and the switches. This underlines the value in minimizing the latency in these elements as industrial systems move toward gigabit speeds, control cycle times reduce (EtherCAT® has demonstrated 12.5µs cycle times), and node count expands with the addition of Ethernet- connected sensors in the control network and the flattening of network topologies. Conclusion In high-performance, multi-axis, synchronized motion applications, control-timing requirements are precise, deterministic, and time-critical, with a requirement to minimize end-to-end latency, especially as control cycle times get shorter and control algorithm complexity increases. Low-latency PHYs and embedded cut- through switches are important elements in optimizing these systems. To address the challenges outlined here, Analog Devices has recently released two new robust Industrial Ethernet PHYs, the ADIN1300 (10Mb/100Mb/1Gb) and ADIN1200 (10Mb/100Mb). To learn about ADI's Chronous™ portfolio of Industrial Ethernet solutions and how they are accelerating real-world Industrial Ethernet networks, visit analog.com/chronous. ADuM4122 Isolated Gate Drivers LEARN MORE ADuM4221 family Half Bride Gate Drivers LEARN MORE ADuM7702 16-bit Sigma-Delta Modulators LEARN MORE LTC7061 100V Half Bridge Driver LEARN MORE ADUM7704 16-Bit Isolated Sigma-Delta Modulators LEARN MORE

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - Industry 4.0 and Beyond