Supplier eBooks

Analog Devices - Energy Storage Solutions: Saving Power for the Future

Issue link: https://resources.mouser.com/i/1437660

Contents of this Issue

Navigation

Page 9 of 27

10 ADI | Energy Storage Solutions Figure 3 illustrates a typical solar system with input-for-input DC strings, DC-to-AC conversion, energy charging and storage, and battery management and communications. Analog Devices offers a complete power, communication, and control interface signal chain solution for solar PV and energy storage applications. iCoupler isolated gate driver solutions include the ADuM4135 and ADuM4223/ADuM3223; iCoupler isolated communication port solutions include the ADM2795E, ADM2587E, and ADM3054. 1 Solar generation, energy storage, and domestic consumption in a typical 24-hour day. Table 1: Domestic Energy Storage Strategies Definition Minimizes electricity purchases during peak electricity consumption hours, while TOU shifts purchases to lower rates behind the meter customers. The goal of this strategy is to reduce the customer's bill. Minimize the export of electricity generated by behind-the-meter PV systems to maximize the financial benefits in PV areas where utility rates are high. Reduce costs when utility companies charge excessively during peak times so customers can store energy. This is a more common strategy and is the charging of any storage capable devices to use when the grid is down or at night time. This is more a backup power strategy, where low utility charges are available at peak times and there is a low feed-in tariffs. Domestic Energy Storage Strategy Bill Management Time of Use (TOU) PV Self Consumption Demand Charge Reduction Backup Power RS-485 has several uses, the primary use being remote monitoring of power generation, power point trackers, and energy storage status (battery storage). For solar applications such as energy storage communications is critical, as it alerts the user of power generation and consumption activities within their solar installation. Several systems strategies can be installed such as bill management, PV self- consumption, demand charge reduction, and backup power (Table 1). Backup power is the most popular, especially in the U.S., because of the various hurricanes causing havoc in the states of Texas and Florida. Solar generation, energy storage, and domestic consumption in a typical 24-hour day is illustrated in Figure 1. Figure 1 shows the primary reason why systems are designed for bill management in a solar system. During nighttime when there is no irradiation on the solar panel, energy consumed will be purchased from the grid where the grids are lowest. As soon as the sun rises, irradiation appears on the solar panels, power is generated, and domestic self-consumption begins where any solar generation is either used in the household or is diverted to charge the energy storage unit. This allows bill costs to be controlled by reducing the energy drawn from the grid and using solar-generated energy where low feed-in tariff areas are available from utility companies. RS-485 is the communication application of choice for PC screen data updates such as current power, current consumption in the maximum power point trackers, battery charge and health, and CO 2 reduction, etc., are available, as can be seen in Figure 2.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - Energy Storage Solutions: Saving Power for the Future