Supplier eBooks

Bourns - How to Choose the Right Surge Protection Technology

Issue link: https://resources.mouser.com/i/1437723

Contents of this Issue

Navigation

Page 23 of 29

24 Making the Right Surge-Suppression Technology Choices "It can be said that the production costs of inserting adequate protections should always be commensurate with the cost of returns from the field, as well as with the level of customer satisfaction." Ivan Fumagalli, Project Manager, Robertshaw Within each technology type is a range of components that vary in their voltage, power, operating temperature ranges, and other electrical specifications. To choose the right surge protection components for a given application, you must minimally determine the following elements: • Maximum continuous operating voltage; maximum reverse working voltage. Choose a component with a maximum rated voltage that is higher than the line voltage. • Peak current. Choose a value larger than the maximum current that will flow during a surge event; measured in amps. • Peak power. Choose a value larger than the peak power that a surge event generates; measured in watts. • Clamping voltage. Choose a value that is below the minimum voltage that the downstream circuitry can withstand during a surge event. In practice, these calculations are complex. Also, most surge-suppression solutions work in conjunction with other surge- and current-limiting technologies installed internally and externally to a facility. Because of the many physical and economic factors involved in choosing the right technology, consider support from a component vendor so that you can make the best choices.

Articles in this issue

view archives of Supplier eBooks - Bourns - How to Choose the Right Surge Protection Technology