Supplier eBooks

Intel - Reimagining What's Next

Issue link: https://resources.mouser.com/i/1437726

Contents of this Issue

Navigation

Page 22 of 37

AI in Image Processing In the signal-processing pipeline, sitting behind the camera optics and the sensor, commercialization of machine learning (leveraging deep neural networks) is enabling a revolution in the way images are constructed and information is subsequently extracted from them. One example can be seen in the use of AI to significantly improve low-light performance, enabling high-quality images to be taken in near-dark conditions. Raw data captured under low-light conditions is known to challenge traditional signal-processing pipelines. Electronically raising sensor sensitivity (ISO number) can add noticeable noise to images resulting in poor image quality, and applying de-noising to the image has only limited effectiveness. Other techniques to improve image quality include extending the exposure time, although this is often impractical in industrial applications or cameras on board vehicles. More recently, an ingenious technique has been developed that leverages machine learning to greatly reduce the detectable noise in images constructed from raw low-light data. A deep neural network is trained using datasets that contain raw short-exposure low-light images and corresponding long-exposure reference images. When the network is fully trained, it is capable of creating high-quality images by working directly on raw short-exposure data. This technique is coming into the market in top-of-the-range smartphones – enabling delivery of better-looking photographs. It is also applicable to capturing better images for industrial and security applications, such as production line inspection or surveillance systems. Conclusion Numerous technical improvements are being developed throughout modern image processing systems – from the camera lens at the front end of the system to the image sensing and image processing apparatus behind it. Together, these are expected to drive expansion in the breadth of applications that can be addressed, as well as increasing system performance benchmarks. 23 INTEL 2020 Global shuttering improves image sharpness when photographing fast-moving objects or when the camera is mounted on a moving vehicle. First featured in high- end still cameras, the technique is now in demand to enhance the performance of industrial and automotive vision systems. In global shuttering, the charge value of all pixels is stored simultaneously to a small in-pixel memory before being read sequentially into the frame buffer line by line as before. This results in a clear image, free of rolling-shutter distortion. Several challenges have been overcome to create global-shutter image sensors that achieve elevated SNR and dynamic range without increasing pixel size to compensate for the presence of in-pixel memory, which effectively reduces the pixel area that can be used for photon absorption. An example of such image sensors is the 1Mpixel, 1/4-inch format ON Semiconductor ARO144. Global shutter pixels feature high quantum efficiency to ensure fast charging while at the same time remaining insensitive to charging effects not related to the image, such as crosstalk resulting from electron diffusion. In addition, optical shielding is applied close to the sensor to exclude stray illumination from the pixel surface. Figure 2: The ARO144 image sensor from ON Semiconductor. Learn More ADLINK TECHNOLOGY PCIE-GIEIMX AI FRAME GRABBER

Articles in this issue

Links on this page

view archives of Supplier eBooks - Intel - Reimagining What's Next