Supplier eBooks

Littlefuse - Circuit Protection for High-Speed Serial Interfaces

Issue link: https://resources.mouser.com/i/1437732

Contents of this Issue

Navigation

Page 5 of 33

6 Circuit Protection for High-Speed Serial Interfaces TODD PHILLIPS | Littelfuse, Inc. These GENERAL PORTS Protect Against Electrical Stress • Static electricity: We typically refer to it as electrostatic discharge (ESD), which commonly comes from human touch. Effectively, we become the source of electrical stress that can damage sensitive electronics. • Short circuits: They are typically caused by things such as a power cross. A power line faulting into a data line or a power line faulting to ground and bypassing the load and that short circuit creates a spike in current that could damage a piece of electronics. • General overvoltage events: These events occur from everyday activities such as turning on motors or lights. Inductive load-switching can wear out electronics over time, cause damage, and need protection. P orts provide a connection to the outside world, primarily for a device looking for data or power. Ports create an opening that becomes an easy entry point for electrical stress (Figure 1). Common electrical stress points would be lightning strikes to a power line that might be traveling down the power line itself and into the device. It could even strike nearby and induce a voltage spike on the power line or even the data lines that need to be protected. Other types: General Port Protection Littelfuse and Mouser Electronics

Articles in this issue

Links on this page

view archives of Supplier eBooks - Littlefuse - Circuit Protection for High-Speed Serial Interfaces