Supplier eBooks

Littlefuse - Circuit Protection for High-Speed Serial Interfaces

Issue link: https://resources.mouser.com/i/1437732

Contents of this Issue

Navigation

Page 20 of 33

21 littelfuse.com LEARN MORE LEARN MORE Littelfuse P-0S-LRP Voice-DS1 SIDACtor ® Protection Thyristors Littelfuse 461 TeleLink ® Surface Mount Fuses PoE Protection Power over Ethernet (15.4W), PoE+ (30W), PoE++ (90W)) powers remote devices via the Ethernet cable (Figure 5). Littelfuse suggests that designers employ TeleLink fuses for overcurrent protection, such as the 461 series. For voltage protection, Littelfuse suggests that one utilize a TVS diode. TVS diodes can be used across the center tap signal pair and a second one across the center tap spare pair. The TVS diode can be chosen based on one's search needs for the specific application. We have 400W, 600W, 1500W, or 3kW. The TVS diode array Littelfuse recommends you looking at is the SMCJ series. For any Ethernet application, the optimal protection depends on where it's being used and the amount of exposure that that location might have to electrical hazards. Standard GR-1089 provides an excellent reference to what testing could be done to select the right components and know that one has adequate protection. One of the tests, GR- 1089, requires a power cross test in how the circuit is protected. It requires a solution such as the 461 fuses, which can not only protect for a power cross event as a short circuit type of event, but it would also be able to withstand the surge levels that are adequate for that outdoor connector. SIDACtors provide surge protection on the lines that have the power. Ghost power created on PoE gets separated off and fed into a power controller to be used as real DC power, and those lines are protected primarily by a SIDACtor. Littelfuse is the company to go to for solutions to protect industrial communication equipment. Whether you rely on RS-485 and Ethernet connections, its wide variety of protection solutions keep your systems up and running in even the most challenging environments. ■ " " Figure 5: PoE Port Protection. (Source: Littelfuse) For any Ethernet application, the optimal protection depends on where it's being used and the amount of exposure that that location might have to electrical hazards.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Littlefuse - Circuit Protection for High-Speed Serial Interfaces