Supplier eBooks

Littlefuse - Circuit Protection for High-Speed Serial Interfaces

Issue link: https://resources.mouser.com/i/1437732

Contents of this Issue

Navigation

Page 7 of 33

8 Circuit Protection for High-Speed Serial Interfaces Figure 2: Littelfuse circuit has a wide selection of protection solutions for power and communication ports (Source: Littelfuse) Across the top of the chart are listed various ports based on data speed, from the slowest on the left side to the fastest on the right. Along the bottom, one will observe two technology types—over-voltage solutions in blue and overcurrent protection technologies in green. The chart reveals which technologies to first consider when looking for optimized port protection. Littelfuse can help to further select parts based on the unique specifications of a particular end-product design. Ethernet Protection for ethernet ports varies based on the level of exposure to electrical hazards. For indoor applications with minimal exposure to potential hazards, a single ESD protector can be sufficient. A single diode array placed after the transformer, such as the SRV05 Series diode array can protect the Ethernet PHY in this case. If one moves outdoors, the environment will be harsher, increasing the risk of receiving damage because of an electrical hazard. A fuse is needed to help protect during a power-cross event when the power line makes contact with the communication lines. Additionally, a Gas Discharge Tube (GDT) such as the CG6 will help protect against dangerous surge events associated with lightning strikes. A diode array, such as the LC03, then adds another level of protection, further clamping the surge and protecting the PHY from damage. RS-485 The protection of an RS-485 line varies by exposure levels. For indoor or intra-building applications, a polymeric positive temperature coefficient device (PPTC) and diode-array combination will provide sufficient over- current and over-voltage protection, however, if the port connects outdoors, such as a rooftop unit, such as a heating, ventilation, and air condition (HVAC) condenser unit. A higher level of surge protection is needed and provided by using a coordinated protection scheme with GDTs and SIDACtors. A PPTC provides overcurrent protection and acts as a coordinating element between the GDT and the SIDACtors. The PPTC ensures that the SIDACtor reacts first, providing fast protection until the GDT can react. CAN, LIN, SIM, µSIM As automotive electronics, or the use of electronics in automotive, have increased, so has CAN and LIN bus prevalence. These communication lines require ESD protection, typically provided by diode arrays. For these automotive-related applications, it is important for all electronic components to pass the rigorous standards of AECQ and its included tests.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Littlefuse - Circuit Protection for High-Speed Serial Interfaces