Supplier eBooks

Maxim - Empowering Design Innovation for Healthcare Wearables

Issue link: https://resources.mouser.com/i/1437735

Contents of this Issue

Navigation

Page 6 of 27

7 Maxim Integrated | 2020 Developing the Heart Rate Monitor Working with Mbed If you have an existing Mbed account, use the Mouser HRM Mbed repository and import the provided code into your compiler. For first-time users: 1. Go to www.Mbed.org. 2. Click the Mbed OS link, which will take you to the developer site. 3. Click Log in/Sign up and provide the required information. Once registered, you can either begin a new project by selecting the highlighted Compiler link or by accessing the Mouser HRM Mbed repository and importing the code to the compiler. You can select, review, add, or change platforms within the Compiler screen by clicking the link in the top right corner. You will find several other Maxim products and software samples also supported through Mbed. Wiring the Board and Reference Design Wiring the MAX32630FTHR and MAXREFDES117 together requires only a few connections and can be breadboarded to make this easier. To do so, use the following steps: 1. Connect the SCL and SDA lines from the heart rate sensor with P3_5 and P3_4 on the MAX32630FTHR and the INT on the heart-rate device to pin P3_0 (Figure 3). 2. The V IN for the heart rate sensor needs between 2.5V to 5.5V, but I recommend deriving power from the 3V3 or SYS connected with the battery. I've had several issues between the two when attempting to use 5V. 3. Connect your ground pin. Programming the Board Programming the board is as easy as dragging and dropping a file from one folder to another. The MAX32630FTHR ships with a debug interface used for uploading your code to the board. Figure 3: Pin mapping from Maxim MAX32630FTHR datasheet Programming the board is as easy as dragging and dropping a file from one folder to another. ""

Articles in this issue

Links on this page

view archives of Supplier eBooks - Maxim - Empowering Design Innovation for Healthcare Wearables