Supplier eBooks

Renesas - 7 Experts on Brushless DC Motor Control

Issue link: https://resources.mouser.com/i/1437741

Contents of this Issue

Navigation

Page 12 of 25

13 This drive type is more expensive than the trapezoidal approach. The third type of drive is the FOC. FOCs rely on measuring and adjusting stator currents so that the angle between the rotor and stator is always 90 degrees. This approach is efficient at high speeds and performs well during dynamic load changes. It also produces minimal torque ripple, so the motor runs smoothly at high and low speeds. Of the three drive types, FOC is the most difficult and expensive to implement. Drive Type Trapezoidal Simple to use Inexpensive Torque ripple at every stage Smoother power delivery Reduced torque ripple More precise motor control Must accurately determine rotor position Accurate current control required Expensive Require accurate measurement and adjustment of stator currents Most difficult to implement Expensive Efficient at high speeds Performs well during dynamic load changes Produces minimal torque ripple Sinusoidal FOC Advantage Disadvantage Chapter Two: Motor Controllers and Drivers Table 1: Summary of BLDC Drive Type Advantages and Disadvantages "Efficiency and safety are the most important factors when choosing a BLDC motor drive. This includes over and undervoltage protection, overcurrent protection, and one-shot high- current protection." Bhanu Villuri Lead Project Engineer, Stanley Black & Decker, Inc.

Articles in this issue

view archives of Supplier eBooks - Renesas - 7 Experts on Brushless DC Motor Control