Supplier eBooks

Renesas - 7 Experts on Brushless DC Motor Control

Issue link: https://resources.mouser.com/i/1437741

Contents of this Issue

Navigation

Page 5 of 25

6 Chapter One: Brushless DC Overview Brushless DC (BLDC) motors are permanent-magnet, synchronous motors that convert electrical power into mechanical power. BLDC motors work according to the attraction and repulsion principle of magnetism, along with the Lorentz force law, which states that force is created when a current-carrying conductor is placed in a magnetic field. As Figure 1 illustrates, BLDC motors have a simple design, with two primary features: • A rotor with two permanent magnets: one positive and one negative • Stators with coil-winding armatures that create a magnetic field when switched on BLDC operation begins with the controller, which has two primary functions. First, the controller receives data about rotor position, which is critical to the motor's operation. Brushless DC Overview Chapter One "Precise motor position information enables us to drive the motor with high torque." Bhanu Villuri Lead Project Engineer, Stanley Black and Decker, Inc. Figure 1: In BLDC motors, magnetic interactions occur between each stator's coil windings and the rotor's permanent magnets. (Source: Renesas)

Articles in this issue

view archives of Supplier eBooks - Renesas - 7 Experts on Brushless DC Motor Control