Supplier eBooks

TE Connectivity - Proven in the Harshest Environments

Issue link: https://resources.mouser.com/i/1437747

Contents of this Issue

Navigation

Page 16 of 37

mouser.com/te-connectivity 17 LEARN MORE LEARN MORE > > TE Connectivity / DEUTSCH HD Harsh Environment Connectors TE Connectivity / DEUTSCH DT Family Connectors Years of operarion Salt per liter of water 40+ 35g The challenge for TE Connectivity was to design, test, and manufacture several fire-resistant cable joints in a limited time that could be quickly and easily installed. THE SOLUTION With many years of expertise and experience in designing and supplying products for demanding environments, TE Connectivity rose to the challenge. It implemented an accelerated development program to design, test, and manufacture a range of rugged, high-performance, and long-lasting products. The program resulted in the development of a wide range of fire-resistant LV and MV joints for control, communications, and power cables that satisfied the customer's stringent specifications. THE RESULT The resilience and reliability of these specially engineered TE Connectivity solutions are born because they are still in operation more than 40 years after they were installed. ■ Harsh Environmental Resistant Cable Joints for Shipbuilding and Offshore BACKGROUND The North Sea presents some of the harshest operating conditions for marine installations and products. The average temperature in the North Sea during the summer months is 17°C while in winter, a season of frequent gales and storms, the average temperature is 6°C while salinity averages 34g to 35g of salt per liter of water. THE CHALLENGE The average temperature in the North Sea during the summer months is 17°C while in winter—a season of frequent gales and storms—the normal temperature is 6°C while salinity averages 34g to 35g of salt per liter of water. The North Sea is also prone to storm surges, an offshore rise of water associated with a low-pressure weather system caused primarily by high winds pushing the ocean's surface. The early days of exploration and recovery of North Sea offshore oil in the 1970s called for exceptionally enduring products that would meet the exacting requirements of the companies operating in this harsh environment. A well-known British oil and gas company, an early leader in the industry, was looking for high-performance low-voltage (LV) and MV joints and terminations for their innovatively constructed platforms.

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - Proven in the Harshest Environments