Supplier eBooks

TE Connectivity - Proven in the Harshest Environments

Issue link: https://resources.mouser.com/i/1437747

Contents of this Issue

Navigation

Page 28 of 37

mouser.com/te-connectivity 29 Testing and Validation Technology and design developed by TE Connectivity have been tested with the sensor package exposed to saltwater, chlorine water, and diiodomethane (methylene iodide, MI) gas. Diiodomethane exposure has been shown as the harshest test. The figures below illustrate the drift in signal output of the sensing element concerning the diiodomethane and chlorine water exposure. The drifts are considered very limited. Additionally, the drift in offset can mainly be explained through the presence of the humid environment rather than the diiodomethane in it. Another accelerated life test, at 85°C and in 85 percent relative humidity (RH), showed the same drifts in offset and span, as plotted alongside the diiodomethane results. LEARN MORE > TE Connectivity M12 Industrial Ethernet Cable Assemblies FIGURE 7: Chlorine test results. (TE Connectivity) CHLORINE TESTING (FIGURE 7) Test Conditions and Procedure: • Samples fully submerged in a chlorine solution at 60°C for 6 hours • Dried in a temperature/humidity chamber at 60°C and 60% RH for 18 hours • Test and record data • Repeat steps 1–3 until 40 cycles are completed • Repeat steps 1–4 at increasing levels of chlorine concentration (from 20ppm to 100ppm) • Samples were compared with standard packaged sensors (not enhanced for harsh media).

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - Proven in the Harshest Environments