Supplier eBooks

TE Connectivity - Building Intelligent Automation

Issue link: https://resources.mouser.com/i/1442385

Contents of this Issue

Navigation

Page 14 of 18

15 Use To simplify the mechanical aspects of this design, we are using a simple linkage that translates the move of the servo arm directly to the manual lever of the damper. The sensor device can be placed anywhere in the room since it is a standalone device. This is helpful so that it can be placed away from air registers or windows that might inadvertently affect sensor readings for the purpose of regulating room temperature. The Huzzah is powered with a standard micro-USB DC power supply—the same kind that power many of today's smartphones and other portable electronics. The weather shield stack is powered with a 5V DC barrel jack power supply. Power supplies that provide sufficient power are included in the project shopping cart for your convenience. Of course, this project could be altered to fit any number of scenarios or system configurations. For example, instead of opening and closing dampers, the system could be repurposed to open and close window blinds based on temperature. Or this could be done in addition to the damper control by simply adding a second control unit. The possibilities are endless. Other Resources Are you interested in building this project yourself or using it as a starting point for further development? If so, we have put together a few resources to help. Building Automation GitHub YouTube Video Mouser.com Shopping Cart If you do build this project or make modifications to it, we would love to see the results. You can find us on Twitter, Facebook, and Google+.

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - Building Intelligent Automation