Supplier eBooks

Analog Devices - The Internet of Things

Issue link: https://resources.mouser.com/i/1442787

Contents of this Issue

Navigation

Page 7 of 27

IoT absolute Off-Shaft Angle of a motor. For instance, the Analog Devices ADA4571 Integrated Anisotropic Magnetoresistive (AMR) Angle Magnetic Sensors & Signal Conditioner provides precise motor shaft angle measurement and can replace high- cost resolvers and optical encoder sensors. These sensors help lower system cost, size, and weight while improving measurement robustness. Most times a mercury thermometer is not going to cut it. The extreme accuracy (0.1°C) of the Analog Devices Inc. LTC298x Digital Temperature Measurement Systems allows for precise temperature measurements in noisy environments. An analog signal provided by a sensor must be converted into a digital signal. An analog-to-digital converter (ADC) is a system that converts this. Its complement is the digital-to- analog converter (DAC), which does the reverse function. ADI is the leading provider ADCs and DACs in the world. ADCs and DACs help the process of converting sensed information into quantitative measured information. For example, the Analog Devices AD7124 Analog Front End (AFE) Portfolio features low power, low noise, completely integrated AFEs for high precision measurement applications. The devices contain a low noise, 24-bit sigma-delta (e-Δ) analog-to-digital converter (ADC). An on-chip low gain stage ensures that signals of small amplitude can be interfaced directly to the ADC. It takes what has been sensed and handles it as quantified information. Sensors are the electronic components used to measure physical phenomenon. By taking analog data from the external world of things it provides a measurement. This measurement is placed from the external world into the digital domain where it can be handled and manipulated further in order to come to a proper interpretation of what the data means. Sensing and measuring are the beginning steps in IoT. Interpreting Interpretation is the art of properly receiving communication and processing it in the manner it was intended for by the communicator. Proper principles of interpretation allow all forms of communication, whether verbal or nonverbal, to be articulated, explained, explicated, or expounded, allowing meaning to be conveyed and understood. The circumstances surrounding the specific grammar, syntax, and discourse employed are called the context. It provides the external and internal environment into which the information is being processed. ADI enables interpretation to happen by bridging the physical and digital with unmatched technologies that sense, measure, and connect. One example of interpretation is an adaptive contactless condition monitoring solution that employs artificial intelligence (AI) to interpret and respond properly to sound and vibration that is sensed and recognized. OtoSense is a software technology platform that turns any machine sounds and vibrations into actionable meaning at the edge. OtoSense does so in real-time. Machine learning (ML), a subset of AI techniques, uses algorithms to extract information from raw data and represent it in a model. The machines learn over time through feedback received through gaining knowledge by studying and experiencing the results of its actions and their associated consequence. Machine learning then adjusts its own internal algorithms in order to acquire fresh and better structural descriptions from the provided feedback. This ML engine may be optimized to detect different machine sounds and vibration profiles. An end-to-end solution, meaning from sensor-to-cloud, may be used for a variety of industrial applications. These include predictive machine health maintenance applications such as heating, ventilation, and air conditioning (HVAC), jet 8 ADXL100x MEMS Accelerometers ADuCM4050 ULP Microcontroller Learn More 4 Learn More 4 • 52MHz ARM ® CORTEX™-M4F with FPU and MPU • Collection of digital peripherals, embedded static random access memory (SRAM) and embedded flash memory • Offers class leading, ultra low power active and hibernate modes • Single in plane axis accelerometer with analog output • Full-scale ranges of ±100g (ADXL1001), ±50g (ADXL1002), ±200g (ADXL1003), and ±500g (ADXL1004) • Ultra-low noise densities from 25μg/√Hz to 125μg/√Hz, over an extended frequency range IoT

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - The Internet of Things