Supplier eBooks

Analog Devices - The Internet of Things

Issue link: https://resources.mouser.com/i/1442787

Contents of this Issue

Navigation

Page 12 of 27

Developers can use these devices to quickly implement sensing systems with few additional components. For simple applications, developers need to do little more than connect a sensor transducer to the AFE's analog input, add decoupling capacitors, and connect a microcontroller (MCU) to the device's serial output. The bidirectional analog ports further simplify their use with resistive sensors such as strain gauges or RTDs that typically required in process-control applications. Developers can use an AD7124-4 analog pin to provide the excitation current needed to drive these sensors (Figure 1). For custom signal chains, developers can augment their designs with low-power devices needed for specialized signal conditioning or conversion. For precision measurements, Analog Devices' ADA4051-1, ADA4051-2, and LTC2063 consume only microamps of current, offering zero-drift op amps with very low offset voltage, drift, and input bias current. Developers can pair these op amps with conversion devices such as the AD5592R or AD5593R, which integrate a 12-bit ADC and 12-bit Digital-to- Analog Converter (DAC) accessible through an SPI (AD5592R) or I2C (AD5593R) interface. Increasingly, however, developers can find AFEs developed to meet requirements in specific application areas. For example, Analog Devices' AD823x integrate a complete signal chain for bio potential measurements including electrocardiograms (ECGs) and electromyograms (EMGs) used in wearable heartrate monitors, gaming peripherals, and other personal products. Even with their extensive functionality, the devices allow developers to meet tight power budgets in designs for wearables or other personal electronics. For example, developers can set the AD8233 in a low-power mode, consuming less than 1μA of supply current, rapidly returning to full-power mode when electrodes are detected (Figure 2). System Power Optimization The ability to tune designs for specific power and performance targets is an essential feature for every component in an IoT design. Perhaps nowhere is this capability more important than in the design's MCU, which typically accounts for most power consumption in any system. With an MCU, the need to maintain some level of functionality has traditionally complicated 13 Figure 1: Designers need few additional components to implement sensor designs with Analog Devices' AD7124-4, even using an analog pin to drive the excitation current needed with resistive sensors while using other analog inputs for sensor voltage measurement and for reference voltage measurement in ratiometric conversion. (Source: Analog Devices) Figure 2: Application-specific AFEs such as Analog Devices' AD8233 support low-power design with capabilities such as quickly transitioning to active mode upon detection of electrodes. (Source: Analog Devices) EVAL-ADICUP3029 Development Learn More 4 • ADuCM3029 Ultra Low Power ARM Cortex-M3 MCU with Integrated Power Management • Arduino Uno R3, Pmod, and Grove I2C compatible connectors • Low energy Bluetooth and Wi-Fi connectivity IoT

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - The Internet of Things