Supplier eBooks

Silabs - Connectivity for Building Home Automation

Issue link: https://resources.mouser.com/i/1442793

Contents of this Issue

Navigation

Page 12 of 21

13 As the Bluetooth connection interval is reduced, the number of Bluetooth connection events increase, and the Zigbee throughput decreases due to the decreased radio time on the Zigbee network. Note that 100% end-to-end message reliability was achieved and, although throughput decreased due to longer data transfer, no Zigbee application messages were lost. To verify the impact of advertisement intervals the device was configured to transmit Bluetooth advertisements at varying intervals instead of maintaining a Bluetooth connection. Since Bluetooth advertisements packets are larger than Bluetooth connection keepalives, they have a slightly higher impact on Zigbee throughput for the same time interval. Advertisement intervals as short as 0.5 seconds have little impact on Zigbee throughput and should meet the needs of most use cases. Designing Systems with Multiprotocol Connectivity With dynamic multiprotocol hardware and software it is now feasible to combine the benefits of multiple protocols in cost effective manner on a single SoC. Home automation, asset tracking, and retail advertising can benefit from combining Zigbee and Bluetooth connectivity on a device. Each device and application has unique needs that require software configurability of items such as Bluetooth connection intervals. Before embarking on development is important to ensure the underlying software and hardware architecture is designed for effective resource sharing of the radio and enables advanced scheduling scenarios. In addition, testing and performance benchmarks should be defined with the specific application and system use cases in mind to ensure proper operation in the field. Figure 5: Zigbee throughput vs. Bluetooth connection interval Figure 6: Zigbee throughputs vs. Bluetooth advertisement interval Enhance Home and Building Automation with Multiprotocol Wireless Connectivity Smart lighting has experienced notable success in home and building automation thanks to a wide selection of application-specific wireless protocols. During this webinar, we'll discuss the wireless technologies that best serve smart lighting, homes, and buildings and consider the benefits of enabling simultaneous operation of Zigbee and Bluetooth low energy (BLE) on a single device. By Tom Pannell, Senior Director of IoT Marketing, Silicon Labs

Articles in this issue

Links on this page

view archives of Supplier eBooks - Silabs - Connectivity for Building Home Automation