Supplier eBooks

Bourns - Circuit Protection Simplified

Issue link: https://resources.mouser.com/i/1442796

Contents of this Issue

Navigation

Page 15 of 33

cable, carrying nearly an amp of current on each twisted pair in the latest spec, while still allowing for 10GBASE-T data transfer. While an impressive spec, users will need to be cognizant of potential heat effects taking advantage of this new capability. Circuit Protection So how does one protect vital equipment from power spikes without interfering with the communications that allow these devices to work properly? This might seem like a challenge to system designers who are very good in their particular areas, but would rather not be bothered with—and might even consider neglecting—such important protections. The good news is that Bourns already has multiple reference designs ready to fulfill this role in the form of their PortNote ® solutions. Their first PoE reference design is meant for 10/100 Base-T Powered Devices (PD) and provides both ESD and overcurrent protection. This reference design includes a Transient Voltage Suppression (TVS) diode array, a pair of bridge rectifiers, a single TVS diode, and a transformer. Bourns also provides a design that protects PSE, including the same TVS diode array and transformer as the PD solution, but adds a resettable fuse, and does not use a single diode or bridge rectifier as in the other design. On a slightly different note, Bourns does have a solution ready for traditional Ethernet connections where ESD is a threat. While somewhat out of the scope of this article, it could be a good design to consider for other wired Ethernet applications. Whatever solution is expedient for an application, these PortNote designs give an excellent starting point for Ethernet protection. Once properly integrated into either a PD, PSE, or traditional wired Ethernet device, this will make for a seamless installation that end users never have to think about. While PoE will initially work with or without this kind of circuit protection, it's important to think about how things could go wrong once installed, and the expense and potential reputation damage when dealing with returns. As PoE usage increases, especially in rugged industrial, automotive, and security applications, designing a hardened product that is as, if not more, reliable than using AC "mains" power will be essential going forward. | 16 | Digi ® XBee ™ Cellular LTE Cat 1 Digi ® XBee ™ Cellular LTE Cat 1 MULTIFUSE ® PPTC RESETTABLE FUSES BMS ISOLATION TRANSFORMERS • The space-saving freeXpansion ™ process enables smaller surface mount package sizes • Multifuse ® devices handle larger currents and voltages with improved resistance stability • PPTC resettable fuses provide continuous circuit protection until a fault is removed • Support serial daisy chain/IsoSPI • include common mode chokes for noise rejection for BMS applications • Hi-Pot Isolation Voltage: 4300VDC LEARN MORE 4 LEARN MORE 4 s

Articles in this issue

Links on this page

view archives of Supplier eBooks - Bourns - Circuit Protection Simplified