Supplier eBooks

Bourns - Circuit Protection Simplified

Issue link: https://resources.mouser.com/i/1442796

Contents of this Issue

Navigation

Page 7 of 33

This solution employs MOVs across the AC supply power lines to divert AC power electrical surges away from sensitive components and an ESD suppressor mounted in front of the DC-to-DC converter to mitigate ESD transients. Each of the PoE implementation's power and data lines is protected by a transient current suppressor and each twisted pair is protected by clamping diodes. Finally, all four twisted pairs are protected isolating transformers. It is good design practice to use surface mount devices for suppressors with four-terminal connections to minimize parasitic inductance. Another good design tip is to use ceramic capacitors in parallel and close proximity with TVS diodes particularly when the devices are connected to a power rail. High-current suppressors must be located in the I/O area. Finally, line-to-ground capacitors that could be subject to electrical transients should be rated for voltages above 2kV. These capacitors must also have low ESR at high frequency and low parasitic inductance. The designer has a wide choice of proven circuit protection products from component vendors. Bourns, for example, is a specialist in the sector and offers a portfolio of fuses, TVS diodes, MOVs and specialized proprietary components such as the company's TCS ™ High-Speed Protectors (HSPs). Among the company's latest products are the SM91074AL and SM13100EL transformers with common mode chokes for noise rejection and circuit protection in PoE applications. | 8 | Figure 4: PoE circuit protection implementation suitable for withstanding severe lightning surges. (Source: Bourns, Inc.) PoE's simplicity and convenience has resulted in its use in a range of applications far beyond that envisaged by the specification's designers. But, while transmitting both power and data on a single cable is convenient, it increases the danger of damage to sensitive components from external and power supply electrical transient events. That makes circuit protection in critical installations vital. Component suppliers offer a wide range of blocking, suppression and isolating technology and associated expertise to help the designer implement a suitable degree of protection dependent on their application and PoE specification employed. Conclusion Application example Figure 4 shows a comprehensive PoE protection implementation. This implementation is, for example, capable of mitigating severe lightning surges such as 4kV, 10/700μs transients. Importantly, such an implementation will have minimal impact on signal integrity.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Bourns - Circuit Protection Simplified