Supplier eBooks

Phoenix Contact - Trusted Connections, Trusted Design

Issue link: https://resources.mouser.com/i/1442799

Contents of this Issue

Navigation

Page 13 of 23

Securely Connected with Ease M12 with Push-Pull Fast Locking System By Falk Daniel Clemens, B. Eng., and Dipl.-Ing. Jörg Hohmeier, Industrial Field Connectivity Phoenix Contact GmbH & Co. KG, Blomberg, Germany Lock the new M12 connectors with push-pull fast locking system easily and securely with just one click. Circular connectors in size M12 have established themselves in many industrial sectors—from production to infrastructure projects. The new M12 push-pull system will give users even more advantages—along with simplified handling, it features a high level of mechanical and electrical stability (Figure 1). Originally used in machine building, the success of M12 as a highly versatile solution goes back many years. When it was originally launched, users were looking for a compact standardized interface with cross-manufacturer availability. At that time, there was less focus on the mechanical requirements. Today, users are far more discerning—they predominantly require interfaces that can withstand mechanical influences or reliably transmit high volumes of data. In many cases, they require both of these features simultaneously. On the one Figure 1: The new M12 connectors with push-pull fast locking system from Phoenix Contact lock easily and securely with just one click. (Source: Phoenix Contact) | 13 | | 14 |

Articles in this issue

view archives of Supplier eBooks - Phoenix Contact - Trusted Connections, Trusted Design