Supplier eBooks

Microchip - Control of Anything, from Anywhere with Peace of Mind

Issue link: https://resources.mouser.com/i/1442802

Contents of this Issue

Navigation

Page 11 of 14

| 12 | Embedded control systems typically incorporate a microcontroller (MCU) as the principal active, and sometimes sole, component. An MCU is a self-contained computer-on-a-chip consisting of a central processing unit (CPU), often with onboard non-volatile program memory for program storage, random access memory (RAM) for data storage, and various analog and digital input/output peripheral capabilities. In addition to the microcontroller, a complete embedded control system incorporates application-specific software, various analog, mixed-signal, timing and connectivity products, and non-volatile memory components such as EEPROMs and Flash memory. In common parlance, the phrase bit by bit means that something happens in stages. It comes to be little by little, step by step, slowly, progressively, and steadily over time. In electronics terminology, a bit refers to a binary (0 or 1) digit. Today's MCUs are expressed employing some multiple of 8-bits—for example, 8-bit, 16-bit, 32-bit controllers are today's most commonly employed architectures. The higher the number of bits, the greater the different possible integer values that can be expressed. Math explains how an 8-bit can provide 28 (256), a 16-bit part can yield 216 (65,536), and a 32-bit part may generate 232 (4,294,967,296) distinct values. A Little-bit on 8-bit and 16-bit Controllers in Smart Applications By Paul Golata Smart 8-bit and 16-bit controllers can tackle a wide variety of applications. This article will outline of the design considerations when determining whether an 8-bit or 16-bit controller will suffice for the application. Two (2) common smart controllers will be looked at as specific examples.

Articles in this issue

view archives of Supplier eBooks - Microchip - Control of Anything, from Anywhere with Peace of Mind