Supplier eBooks

NXP - Imagine the Possibilities

Issue link: https://resources.mouser.com/i/1442826

Contents of this Issue

Navigation

Page 13 of 27

I.MX 8X MEK • Platform for evaluation and development of the ARM Cortex® A35 + Cortex-M4F based i.MX 8QuadXPlus, i.MX 8DualXPlus, and i.MX 8DualX applications processors • Kit also provides a platform for NXP PF8100 Power Management Integrated Circuit (PMIC) solution and sensors • Ideal for safety- certifiable and efficient performance requirements LEARN MOREu requisite performance and additionally needed features for these next-generation vision system applications. For example, the integrated automotive-grade hardware accelerators in the NXP S32V2 are ideal for deep neural network processing because they can reduce CPU usage and save computing resources which are critical for applications such as driver monitoring systems. Systems such as these are quickly becoming mandatory. Euro NCAP has made DMS a primary safety function slated for NCAP incorporation by 2020. Driver Monitoring Systems are one of the interrelated parts of advanced driving assistance systems (ADAS) and are essential for Level 3 and higher driving systems. Additionally, the S32V processor supports broader machine learning and sensor fusion applications which are needed in autonomous drive systems. NXP aims at helping automotive engineers develop their applications swiftly by offering a cost- competitive evaluation board and development platform (SBC- S32V234) that can be coupled with NXP software development kits and NXP design studios that are specifically tailored for the S32V processor. NXP is not only dedicated to accelerating time- to-market for Level 3 and beyond automated driving capabilities but also driving toward increased road safety for society. Are you developing with NXP? ■ Notes: 1Based on Strategy Analytics 2019 forecasts I.MX 8-BASED NEURAL NETWORKS FOR OBJECT RECOGNITION 14 AI

Articles in this issue

Links on this page

view archives of Supplier eBooks - NXP - Imagine the Possibilities