Supplier eBooks

Microchip - Concept to Creation

Issue link: https://resources.mouser.com/i/1442841

Contents of this Issue

Navigation

Page 12 of 31

13 / ATSAMW25-XPRO Evaluation Board Figure 4: Left: Brightness at approximately 50 percent. Right: Brightness at approximately 90 percent. (Source: Mouser Electronics) MIC3202 HB LED Driver Evaluation Board • Dedicated dimming control input • ±5% LED current accuracy • 6V to 37V input voltage range LEARN MORE • 33.8mm x 14.9mm compact footprint • ATECC108A CryptoAuthentication™ engine • Over-the-air updates LEARN MORE PROJECT IN ACTION Once the project is assembled, hook up the Xplained board to a computer and fire up a serial terminal (Figure 4). You should see telemetry from the light sensor flowing as well as MQTT messages to and from the Medium One MQTT broker. If not, check to see if there are any error messages. Some common errors include: 1. Mixing up the line, neutral, and ground wires feeding the power supply. 2. Reversing the V+ and V- wires on the power supply or LED driver board. 3. Reversing the LED- and LED+ wires on the LED light strip or the LED driver board. 4. Reversing power and ground wires to sensors. 5. If powering the device, ensure the power supply can deliver at least 1A of current. 6. The wireless network is not running, or SSID or security key was entered incorrectly. " " Medium One provides IoT developers a platform where their IoT devices can communicate and compile data sets from across multiple IoT devices.

Articles in this issue

Links on this page

view archives of Supplier eBooks - Microchip - Concept to Creation