Supplier eBooks

Molex - From here to the Future

Issue link: https://resources.mouser.com/i/1442862

Contents of this Issue

Navigation

Page 22 of 30

| 23 | POWERTRAIN SOLUTIONS MX150 AUTOMOTIVE CONNECTORS Learn more > Learn more > battery electric vehicles (BEV) continue to drive this trend with complex battery management systems with massive amounts of connections and wiring packaged in a small space. This challenge creates the need for solutions that are not traditional to automotive applications, such as micro-sized connectors, very small wire gages, and flexible flat cables (FFCs). Also, the HEV and BEV markets increase vehicle lifespans from a traditional 320,000km (200,000 miles) to 1.6 million km (1 million miles). This creates the challenge of connection systems and terminal contact interfaces that can withstand temperature and vibration over this extended period of time. Molex is a leader in meeting this challenge with ongoing work on contact physics and two-piece terminal designs. This approach provides the robust systems needed electrically and, combined with Molex's exclusive two-piece terminal design and manufacturing capabilities, is providing the robust systems mechanically, as well. Regardless of engine type, whether traditional internal combustion engine, HEV, or BEV, the need for more I/Os near the engine and in harsh environments is increasing. Engine controllers have evolved to become sophisticated computers that are sending and receiving data throughout many systems in the vehicles. Additionally, the transition to smaller systems is also happening with engine controllers as requirements for circuit counts reach more than 300 in such systems. Smaller wires and terminal systems create challenges in operating in environments with higher temperatures and vibration. Besides benefiting vehicle lifespan, Molex's terminal designs and work on plating and contact physics have brought about small terminal systems that can operate in these harsh environments. (Figure 3) Figure 3: With the increasing popularity of electric cars, design requirements for control units and their management are evolving. (Source: Molex)

Articles in this issue

Links on this page

view archives of Supplier eBooks - Molex - From here to the Future