Supplier eBooks

Wurth - Behind the Mystery of Electromagnetic Compatibility Design

Issue link: https://resources.mouser.com/i/1447260

Contents of this Issue

Navigation

Page 9 of 25

Behind The Mystery of Electromagnetic Compatibility Design 10 The result of the calculation is that high interference emissions can be expected. For example, the product family standard EN 55022 can be used here for assessment of the interference emission. In the frequency range of 0.15MHz to 0.5MHz, it defines a permissible Quasi-Peak weighted interference level of 66dBµV to 56dBµV. Figure 2 shows the result of the measurement of the conducted radio interference voltage of this switch-mode power supply without line filter. Design of a Line Filter Figure 3 shows the schematic design of a simple single-phase line filter. Würth Elektronik provides various models of line chokes, such as the WE-CMB series, for the construction of line filters. A line choke basically consists of a MnZn ring core on which two geometrically separated windings are wound in opposite directions. Figure 4 shows the design of the WE-CMB. In this case, the WE-CMB acts as a filter coil that counteracts the current and reduces its amplitude. A common mode choke with as-low-as-possible SRF in the lowest frequency range should be selected because the switch-mode power supply used here switches with very low pulse frequency. Low SRF causes high attenuation in the lower frequency range. The measurement shows that a line filter is absolutely essential. Figure 2: Radio interference voltage of a switch mode power supply without line filter (Source: Würth Elektronik) The measurement shows that a line filter is absolutely essential. "

Articles in this issue

view archives of Supplier eBooks - Wurth - Behind the Mystery of Electromagnetic Compatibility Design