Issue link: https://resources.mouser.com/i/1449105
Improving Lives with Digital Healthcare 26 Personalized Content Immersive technology may be personalized. It may be set up to respond both to the users' personal manipulations and the medical training instructor to accentuate learning in areas where the student may require more attention and focus. It will also provide instructors with the ability to tailor the content fed to the student and respond to their responses, establishing a personalized feedback loop which can be positively positioned and reinforced over time by the instructor or via artificial intelligence (AI). Its convenience allows for self-paced customized training. Figure 3: Medical professions may employ immersive technologies to both learn and service patient needs. Engaging Experience It can feel so real. This is how most people using immersive technology subjectively experience what is happening. While utilizing immersive technologies, their physical senses are led to take their experience as all-encompassing reality, merging the material and the digital realm. Because the student experiences the immersion technology as real and their attention is focused entirely on their environment, they absorb more of it. Just as no one goes to sleep or daydreams while scuba diving, because of the real difference in the contextual experience, the student who learns with immersive technologies will be more highly engaged. Through repeatable practice simulations, the student can develop competency and confidence (Figure 3). Advancing Immersive Technology Molex brings decades of experience in advanced electronics, connectivity, and sensor technologies to help transform medical and pharmaceutical solutions. Molex is an innovative leader in designing, developing, and delivering world-class medical device solutions, including those that will enable the next generation of medical training and learning. Family Gauge (AWG) Pitch (mm) W-W W-B W-P B-B Comments Nano-FiT 20–26 2.5 X X The smallest to date, a fully isolated header that meets customers' power needs while protecting the terminals in a small package Micro-FiT 18–30 3.0 X X X Offers premium housing features to prevent mismating, reduce terminal backout, reduce operator fatigue during assembly, and aid in blind-mating applications Micro-FiT+ 16–30 3.0 X Provides increased current capability compared to other connectors, as well as reducing the mating force by 40% Ultra-FiT 16–22 3.5 X A 3.50mm pitch power connector that supports 14.0A and reduces terminal backout with low mating force; ideal for high- circuit application Mini-FiT Sigma Sealed 12–24 4.2 X Utilizes traditional Mini-Fit TPA2 terminals and wire gauges while protecting from moisture, foam, and dust debris ingress Mini-FiT 16–28 4.2 X X X Mini-Fit Jr. and Mini-Fit Plus Power Connectors deliver up to 9.0A and 13.0A, respectively, while blind-mating, terminal position assurance, and backshell options offer a versatile connector system for a wide range of applications Mega-FiT 12–16 5.7 X X Provides more power per linear and square millimeter than most mid-range power connectors in the industry Figure 4: The FiT product family.