Supplier eBooks

Analog Devices - 12 Experts on Precision Analog Signal Chain Technology

Issue link: https://resources.mouser.com/i/1470437

Contents of this Issue

Navigation

Page 12 of 27

"Today's increasingly complex control system design and corresponding unavoidable increase in signal interference means that DC precision is a must. AC interference in the DC signal results in noisy readings, which can compromise the system." Sneha Patel Senior Power Hardware Engineer R&D, Rockwell Automation Chapter Three Optimizing for Highest DC Precision One of the major optimizations that engineers might desire for their precision signal chain is achieving the highest DC precision. Precision narrow bandwidth signal chains are designed for applications where DC precision is the highest priority, providing best-in-class accuracy, stability, repeatability, and resolution. For the purposes here, the narrow bandwidth signal frequency range is defined as DC to approximately 10 kilohertz (kHz). A source measurement unit (SMU) is an example of an application for which an extremely high level of precision is required at narrow bandwidths. SMUs are closed-loop four-quadrant instruments with sink and source voltage and current capability, and they generate and measure highly precise signals. At a minimum, an SMU must be fast and accurate and feature a wide dynamic range while maintaining stability for a wide variety of load conditions. The accuracy and quality of the instrument produced will be directly impacted by the component selections within the SMU signal chain. Creating a highly accurate, stable, and repeatable SMU places demanding requirements on its signal chain components. However, when tradeoffs are correctly balanced and optimized, incredible DC precision performance can be realized. The key accuracy specifications of an SMU are impacted by the linearity, monotonicity, glitch energy, noise performance, and repeatability of its underlying signal chain. 13 | Optimizing for Highest DC Precision

Articles in this issue

view archives of Supplier eBooks - Analog Devices - 12 Experts on Precision Analog Signal Chain Technology