Supplier eBooks

Analog Devices - 12 Experts on Precision Analog Signal Chain Technology

Issue link: https://resources.mouser.com/i/1470437

Contents of this Issue

Navigation

Page 16 of 27

"Each device has its own set of requirements. Whereas some devices require wide bandwidth, others need rapid response times to perform their functions best." Nishith Patel Principal Hardware Engineer, ABB GISPL Chapter Four Optimizing for Highest Precision with Fast Sampling In other scenarios, engineers might wish to design a precision signal chain for fast sampling or wide bandwidth applications. An example of an application that requires high precision with fast sampling is any closed-loop feedback system, such as hardware-in-the-loop or a source measurement function used in test and measurement instruments. In a system like this, feedback from the output is used as an input, and this information informs the system's decision-making to produce a more precise system. In this case, the latency of the signal chain will contribute to the latency of the whole system—for the best performance, engineers need signal chains that achieve the fastest sampling rate possible, all without sacrificing precision. One aspect of achieving a precision wide bandwidth signal chain is the use of specialized high- precision, fast components such as high-resolution ADCs and DACs featuring high sampling rates. However, for truly fast performance, the chain must be considered holistically, requiring a fast analog front end, filtering stages, and programmable gain stages. Beyond just component selection, other aspects of system design become crucial. For example, as speeds increase, clock jitter can become a limiting factor in a system's performance. Another factor for achieving high precision at fast sampling is the system layout. Good practices such as separating digital and analog systems can have a significant impact on the performance of wide bandwidth signal chains. Tools like LTspice® enable engineers to analyze signal chain noise and transient performance in a simulation environment. 17 | Optimizing for Highest Precision with Fast Sampling

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - 12 Experts on Precision Analog Signal Chain Technology