Supplier eBooks

TE Connectivity - Connected LED Lighting Solutions

Issue link: https://resources.mouser.com/i/1475721

Contents of this Issue

Navigation

Page 5 of 35

6 Connected LED Lighting Solutions FIGURE 2: Features of the LUMAWISE Endurance S (Source: TE Connectivity) Powered upward-facing interfaces have been available for several decades through the ANSI C136.10 interface. This standard was updated many years ago to allow for signal contacts and dimming controls, and C136.41 was created. Now, two-node architecture allows for sensor devices that need a downward field of view. Presently motion sensors are getting released, although other innovations are happening. For example, the Lake Macquarie City Council in Australia organized a hackathon to create sensors for smart-city applications for the two interface luminaires they have installed throughout the city. In many regions, ANSI C136.41 is dominant, and therefore the Zhaga Book 18's third (3rd) edition detailed a hybrid two-node architecture. With an ANSI interface facing upward and a Zhaga interface facing downward in this edition, the wiring of a luminaire gets defined, and the requirements of a control device. Zhaga is now considering the next phase of the book and looking at how it adopts this architecture for form factors other than cobra heads. Heritage lighting is recognized as an essential subset of street lighting and is increasing in popularity but will provide challenges for the two-node architecture. TE supports the Zhaga and ANSI streetlight interconnects platforms. For the Zhaga interface, TE Connectivity offers the LUMAWISE Endurance S product range. It is made up of the receptacle, which mounts to the streetlight, shown on the left of the image below (Figure 2). TE released the second-generation version of that product. It features a dual-wire poke-in, an updated seal for specific mounting configurations, LEARN MORE > TE Connectivity LUMAWISE Endurance S2 Street Light Connectors LEARN MORE > TE Connectivity LUMAWISE Endurance N+ Control Bases & Covers

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - Connected LED Lighting Solutions