Supplier eBooks

TE Connectivity - Connected LED Lighting Solutions

Issue link: https://resources.mouser.com/i/1475721

Contents of this Issue

Navigation

Page 16 of 35

mouser.com/te 17 FIGURE 3: The FB series filters are ideal for most street lighting applications. The EMI filter should be placed as close as possible to the ballast or driver to prevent RF from traveling down the conductors and acting as an antenna. (Source: TE Connectivity) The FB series of EMI filters from TE provides the ideal solution for street lighting issues. This series is approved at 277VAC, which fits into most lighting applications. TE has also obtained UL recognition, along with a UL listing. The FB series also supports solid copper leads, which the lighting industry prefers. Nearly all EMI filters are approved to only 250VAC, making the TE product an immediate solution for lighting customers. The EMI filter should get positioned as close to the ballast or driver as possible (Figure 3). This helps eliminate RF from traveling down the conductors and acting as a transmitting antenna. Conclusion Although the addition of an EMI filter adds cost to the initial overall LED street lighting design, it helps to avoid potential complaints from residents or other users of street lighting that experience interference due to EMI. A complex and costly analysis of the source of the EMI interference can be avoided with this upfront protection. ■ LEARN MORE > TE Connectivity LUMAWISE Endurance S Domes LEARN MORE > Lumileds LUXEON® 3030 2D LEDs

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - Connected LED Lighting Solutions