Supplier eBooks

Qorvo - The Future of Automotive

Issue link: https://resources.mouser.com/i/1484091

Contents of this Issue

Navigation

Page 29 of 35

30 The Future of Automotive paralleling SMT devices is a viable solution. If using two SMT devices in parallel to replace one SMT device, each of the two paralleling SMT devices should have twice the on-resistance compared to using only one SMT device. In this case, the current in each is halved, but on-resistance is doubled for each, so dissipation is half of a single part. The total dissipation of two paralleled SMT devices would be slightly lower compared to using just one SMT device with half the on-resistance. Thermally, each device would be much cooler because for the same thermal management (thermal resistance from junction to ambient or coolant), each paralleling device only dissipates half the loss of a single SMT device. So theoretically, each paralleling SMT device's temperature rise from ambient- or coolant-to-junction should also be half of a single SMT device. Apart from this, the lower package inductance of the D2PAK-7L might allow faster switching edge-rates for even lower dynamic losses. UnitedSiC UJ4C/SC 750V Gen 4 SiC FETs LEARN MORE > UnitedSiC UF3SC 650V and 1200V High-Performance SiC FETs LEARN MORE > A surface-mount alternative would seem attractive, but at the 22kW level? Actually, yes, it can be viable with UnitedSiC (now Qorvo) D2PAK-7L devices with little or no effect on performance, depending on the power conversion stage considered. Looking at the headline differences between the package styles in Table 1 above, the D2PAK-7L wins except for die pad size, which results in an overall junction to cooling fluid thermal resistance of around 1.3°C/W for an 18-milliohm device bonded to an insulated metal substrate, about 30 percent more than the TO-247-4L package. The practical effect of a higher thermal resistance is a higher junction temperature for given power dissipated, all things being equal, but because of the substantial assembly savings with an SMT device, perhaps lower resistance parts can be used, reducing temperature. However, if using only one SMT device reaches thermal limits—Tj becomes too high— Table 1: Comparison between D2PAK-7L and TO-247-4L. (Source: Qorvo)

Articles in this issue

Links on this page

view archives of Supplier eBooks - Qorvo - The Future of Automotive