Issue link: https://resources.mouser.com/i/1490195
Apex 2022 7 Power Operational (Linear) Amplifiers • Designed for applications that require high current and high voltage. • Feature output currents from 0.01A to 100A (peak). • Provides a compact proven solution for demanding precision power analog applications. LEARN MORE PA12 Class A/B Power Amplifiers • 10A, 90V power operational amplifiers with low thermal resistance. • Ideal for applications like driving resistive, inductive, and capacitive loads in motors. • Class A/B output excellent linearity. LEARN MORE manufacturability, and electrical testing. The mid-point of this phase includes the prototype build and post- prototype review, in which Apex engineers complete design verification testing of the device prototypes. Their goal is to test the device's performance against the design concept and project goals, once again checking for flaws and identifying any potential risks. Phase-3 consists of product production tests, readiness review, and a pilot production run. In Phase-3, the device in its production form takes shape. This phase is also extremely important because characterization data are gathered, verified, and finalized into a device datasheet. To exit this phase, no issues can exist with the product's reliability or performance. Next is Phase-4, which is the official product launch and market release—the point at which engineers can find the devices in stock at authorized distribution partners such as Mouser. The last phase, Phase-5, covers market review—a valuable method of receiving feedback from customers who can provide insights into how to make the Apex portfolio of COTS products even better as future designs are considered. Through this entire process, Apex compares its products to the strictest requirements and specifications, ensuring a high-performance, high-reliability power analog solution as the end result. APEX PRODUCTS MEET OR EXCEED THE STRICTEST REQUIREMENTS AND SPECIFICATIONS, ENSURING A HIGH - PERFORMANCE, HIGH- RELIABILITY POWER ANALOG SOLUTION AS THE END RESULT. Winning With COTS For analog power electronics design, high reliability is among the most important considerations. Compared to discrete analog power solutions, COTS solutions can provide a plethora of benefits to the designer in terms of cost, reliability, and time to market. However, for the utmost reliability and performance, the COTS manufacturer must be reliable and reputable. In this regard, Apex Microtechnology has earned its place as a trusted partner to the world's industry leaders. Apex has a legacy of more than 40 years of designing and manufacturing high-reliability integrated power analog solutions to enable, advance, and accelerate the development of high technology for complex electronic systems.