Supplier eBooks

Renesas - Bringing Intelligence to the Edge

Issue link: https://resources.mouser.com/i/1499313

Contents of this Issue

Navigation

Page 22 of 27

Renesas 2023 23 third-party solutions as part of the Arm ecosystem increases the range of choice for application development. This means that developers can choose the software model that best suits their needs while utilizing Renesas's excellent Arm-based silicon solutions as well as speed up the implementation time of complex areas like connectivity and security. Voice Recognition Engine Based on the Renesas ecosystem, Cyberon DSpotter (Figure 3) is a local voice trigger and command recognition solution with robust noise reduction that consumes very low resources and provides high- accuracy performance. It supports multiple languages as well as many connectivity function and security capable depending on the selected MCU. The major features are listed below: • Local voice recognition algorithm, no network connectivity needed • Phoneme-based modeling • Quick command customization—removes the need to collect speech data in advance • Optimization by model adaptation just with small amount speech data • Global language support: 44+ languages worldwide Figure 3: Cyberon DSpotter voice recognition engine. (Source: Renesas Electronics) • Small footprint and cost effective (single DMIC + RA6E1 or RA4E1) • DSMT Tool: wake-word and commands customization, performance tuning, testing, no prior neural network knowledge needed. • Separation of recognition engine and command model, switching commands dynamically • Low-power, high-efficiency RA MCU with strong security function

Articles in this issue

Links on this page

view archives of Supplier eBooks - Renesas - Bringing Intelligence to the Edge