Supplier eBooks

Vishay - The Next Generation of Industry 4.0

Issue link: https://resources.mouser.com/i/1505196

Contents of this Issue

Navigation

Page 9 of 19

10 \ VISHAY Industry 4.0 and Beyond Vishay currently offers 29 different photodetector cells that are 7.5mm in size. The VEMD5080X01 is a low- profile, blue-enhanced, surface-mount version measuring 5mm by 4mm by 0.9mm. The TEMD5080X01 is the most efficient photodiode of this type. It has an opening angle of 130° and generates up to 2mA at 0.52V under 1.5AM, converting with 16% to 19% efficiency. The goal here is to eliminate the situation where battery replacement is required frequently to avoid system malfunctions or failures in the event of an emergency. For example, smart meters often required more power than was predicted on the basis of simulations because the radio connection was weaker than expected or ran into interference. Therefore, the batteries in the field had to be replaced considerably more often than forecast by the manufacturer. Figure 4: The VEML6035 low power, high sensitivity I 2 C ambient light sensor is a board that requires minimum operating voltage 1.7 V only. (Source: Vishay)

Articles in this issue

view archives of Supplier eBooks - Vishay - The Next Generation of Industry 4.0