Supplier eBooks

Microchip Technology - The Mighty 8-Bit Microcontroller

Issue link: https://resources.mouser.com/i/1506681

Contents of this Issue

Navigation

Page 6 of 24

Almost everything electronically operated in a car is now on a network. A centralized ECU knows everything that's happening in the vehicle, and this level of oversight is only possible if you're putting some intelligence out at every single one of those nodes. The result is that every little light bulb and every little switch in a modern vehicle is connected directly to a microcontroller." Jason Layton Senior Applications Engineer, Microchip Technology Inc. C h a p t e r 1 | 8 - B i t f o r A u t o m o t i v e individual modules associated with each system. This architecture allows for decreased design complexity and improved scalability for original equipment manufacturers (OEMs). Taking a closer look at this architecture, you'll find that the modern vehicle setup consists of many individualized subsystems, all of which are connected and governed by larger electronic control units (ECUs). Looking deeper into each of these modules, you'll see that MCUs are a fundamental component at the core of them all. Specifically, common practice is to use MCUs as a means of controlling peripheral functions without adding significant complexity or overhead to the system. The result is that MCUs are critical aspects of almost all modern automotive systems. While many options for MCUs to power these modules are available, in many respects, 8-bit MCUs are the ideal choice. Largely, 8-bit PIC & AVR MCUs are preferred in vehicle subsystems because of their simplicity and efficiency, which help keep the design compact. For these reasons, you'll commonly find PIC 7 The Mighty 8-Bit Microcontroller: Still Enabling Innovation in Modern Applications

Articles in this issue

Links on this page

view archives of Supplier eBooks - Microchip Technology - The Mighty 8-Bit Microcontroller