Supplier eBooks

Littelfuse - 7 Experts on Automotive Powertrains

Issue link: https://resources.mouser.com/i/1516386

Contents of this Issue

Navigation

Page 22 of 32

C h a p t e r 5 What are the differences between onboard charging and offboard charging? To charge batteries found in EVs, engineers can either rely on a charger built into the vehicle (onboard charger) or a charger external to the vehicle (offboard charger). Because onboard chargers are designed to connect to AC mains voltages, rectifiers are needed to convert AC voltage into DC voltage to charge the battery. In addition, the grid connection exposes the vehicle to any transient voltage present on the grid, so protection should be taken into consideration. For offboard chargers, the vehicle is designed to connect to a DC charging point, which keeps the AC/DC conversion away from the EV and directly couples the EV battery to the DC source. Offboard chargers must also integrate communication lines between the vehicle and the charger so that the correct amount of charging current can be negotiated. What advantages does offboard charging present? Some of the biggest advantages of offboard charging include: • Dynamic power flow. Communication cables used between the DC charge point and the EV allow the charger to OFFBOARD CHARGING The increasing popularity of electrical vehicles is boosting the need for efficient and fast charging stations. With some capable of up to 350 kW, we are now getting close to the fueling experience." Philippe Di Fulvio Business Development Manager, EV Infrastructure, Littelfuse 23 7 Experts on Automotive Powertrains

Articles in this issue

Links on this page

view archives of Supplier eBooks - Littelfuse - 7 Experts on Automotive Powertrains