Supplier eBooks

Littelfuse - 7 Experts on Automotive Powertrains

Issue link: https://resources.mouser.com/i/1516386

Contents of this Issue

Navigation

Page 28 of 32

C h a p t e r 6 How do commercial vehicles differ from consumer vehicles? Commercial vehicles require higher system voltages and experience a far higher number hours in operation than passenger cars. Additionally, reliability is essential in any commercial vehicle, especially because a vehicle's commercial value is dependent on its uptime; repair work results in monetary loss. Industrial applications such as mining and construction add challenging requirements regarding vibrations to the design. What are the most common types of power semiconductors found in commercial EVs? Commercial vehicles have several electrical systems utilizing various bus voltages. The 12V-network is used to power electronic systems from sensors and cameras to heated seats and window lifters. In these cases, standard MOSFETs do the power conversion well thanks to their low cost, high reliability, and well-understood operating nature. Outlets providing mains voltages (120VAC/240VAC) are also commonly found in commercial vehicles to provide mobile POWER SEMICONDUCTORS AND OFFBOARD CHARGING FOR COMMERCIAL VEHICLES With the dawn of autonomous trucks, operators will try to get the time for charging down as much as possible— time is money. If it is desired to get those 600kWh into the battery in less than 15 minutes, 2.4MW of power would be required." Martin Schulz Global Principal, Application Engineering, Littelfuse 29 7 Experts on Automotive Powertrains

Articles in this issue

Links on this page

view archives of Supplier eBooks - Littelfuse - 7 Experts on Automotive Powertrains