Supplier eBooks

Murata - 8 Experts on Overcoming Challenges of RF Solution Design

Issue link: https://resources.mouser.com/i/1517877

Contents of this Issue

Navigation

Page 31 of 33

8 Experts on Overcoming Challenges of RF Solution Design 32 "A common way to combat interference among components is to make the device larger, but that is not an option for devices." Erik Jensen Head of Wireless System Integration, Denmark—WSAudiology Working with electronics since his teens, Erik Jensen has always been fascinated by communication and wireless connectivity. For the past fifteen years, he has worked in telecommunication companies, bringing internet connectivity to machine-to-machine equipment, people with hearing loss, and people in remote places without cellular coverage. He believes that information is key and should be available from everywhere and to everyone. Physical configuration of components, radio interference, and power consumption are the biggest challenges when making small wireless devices such as hearing aids. Each of these elements affects the others in the device. When you make a small device, you must put processors, sensors, radio-frequency (RF) components, and power supply close together in the same small package. That design creates a problem for RF immunity because all these different components create noise. A common way to combat interference among components is to make the device larger, but that is not an option for all devices. The issue becomes even more complicated when you have different radios in the same small device. It's not just RF immunity within the device itself, either. The device must be immune from other sources of RF noise in the environment, such as mobile phones, Wi-Fi, and television. Power consumption is another significant challenge, especially in small devices such as hearing aids that must operate for a full day between charges. In normal use, a hearing aid is not always using its RF connectivity functions; however, it consumes the most power when it is transmitting. There's always a trade-off among power consumption, connectivity range, and size. Using a Wireless Chip Protects Against Technology Obsolescence

Articles in this issue

Links on this page

view archives of Supplier eBooks - Murata - 8 Experts on Overcoming Challenges of RF Solution Design